2009-02-17 02:25:27     Writing back to flash

Document created by Aaronwu Employee on Aug 13, 2013
Version 1Show Document
  • View in full screen mode

2009-02-17 02:25:27     Writing back to flash

andy (UNITED STATES)

Message: 69499   

 

Hi

 

Am using BF537 Core module from tinyboards.com. Am using ext2 filesystem. The root file system is loaded onto the ram from the flash. Everytime I make changes to the files or create files they are removed upon reboot. I guess that the changes made are not written back to the flash. How should I get make the changes permenant i.e. reside even after reboot?

 

thanks.

QuoteReplyEditDelete

 

 

2009-02-17 05:44:08     Re: Writing back to flash

Daniele Pagani (ITALY)

Message: 69520   

 

Dear Andy,

 

I think that a good solution is to read here:

 

docs.blackfin.uclinux.org/doku.php?id=linux-kernel:mtd

 

in order to understand Memory Technology Devices.

 

Daniele.

Attachments

    Outcomes