2009-02-13 07:45:25     Alsa driver for SSM2602 with BF53x

Document created by Aaronwu Employee on Aug 13, 2013
Version 1Show Document
  • View in full screen mode

2009-02-13 07:45:25     Alsa driver for SSM2602 with BF53x

Laurent Brard (FRANCE)

Message: 69413   

 

Hi,

 

I am considering interconnecting a BF536 with an SSM2602.

 

I have seen in the 2008R1.5 release that the SSM2602 seems only supported as a System On Chip device in the BF52xC.

 

Still it looks like there are an I2C address and a SPORT between the blackfin and the codec.

 

So I am wondering if I could set up a BF536 with an external SS2602 and still have the driver work almost as is.

 

Thank you in advance,

 

Laurent

QuoteReplyEditDelete

 

 

2009-02-13 07:54:48     Re: Alsa driver for SSM2602 with BF53x

Robin Getz (UNITED STATES)

Message: 69416   

 

Laurent:

 

The SSM2602 inside the BF52x is just two die in the same package - you still connect the pins of the SPORT and the codec externally.

 

It should work without issue on the 536 - if it doesn't it is our fault, and we will fix it.

 

-Robin

QuoteReplyEditDelete

 

 

2009-02-13 07:55:43     Re: Alsa driver for SSM2602 with BF53x

Michael Hennerich (GERMANY)

Message: 69417   

 

The driver works 100% as is.

 

It doesn't matter if the SSM2602 is internal or external.

 

-Michael

Attachments

    Outcomes