2009-02-13 04:12:17     qt-embedded 3.3.5 examples

Document created by Aaronwu Employee on Aug 13, 2013
Version 1Show Document
  • View in full screen mode

2009-02-13 04:12:17     qt-embedded 3.3.5 examples

Patrick Hotz (GERMANY)

Message: 69381   

 

Hi Guys,

 

currently i try to compile konquerror embedded on my uClinux-Board...

 

First i want to try a example from the qt-embedded 3.3.5....

I have followed the steps in  docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:qt&rev=1213628771 with static library....

The qt-embedded is compiled ok, also the examples..

 

Now i have copied the drawline-example and the two other files like the manual on "For FLAT static QT demo" to my system.

Also i have export the QTDIR...

 

If i want to run the example there is following:

 

root:/media> ./drawlines -qws

mapping /dev/fb0: Invalid argument

Error: failed to map framebuffer device to memory.

: driver cannot connect

root:/media>

 

For testing i have enabled the Virtual Framebuffer in Kernel-Settings.

Booting shows this:  fb0: Virtual frame buffer device, using 1024K of video memory

 

Does anyone know a solution to this problem?

 

 

 

Greetings,

 

Patrick

Attachments

    Outcomes