2009-02-06 10:02:51     Compiling Perl..

Document created by Aaronwu Employee on Aug 13, 2013
Version 1Show Document
  • View in full screen mode

2009-02-06 10:02:51     Compiling Perl..

Emanuele Italia (ITALY)

Message: 68994   

 

Hello,

 

i'm tring to compile perl, but i found out this error:

 

v.c: In function ‘Perl_sv_utf8_decode’:

sv.c:2489: warning: unused variable ‘has_utf’

sv.c: In function ‘Perl_sv_setpvn’:

sv.c:2959: warning: unused variable ‘iv’

sv.c: In function ‘Perl_sv_magic’:

sv.c:3345: warning: suggest explicit braces to avoid ambiguous ‘else’

sv.c: In function ‘Perl_sv_unmagic’:

sv.c:3491: warning: suggest explicit braces to avoid ambiguous ‘else’

sv.c: In function ‘Perl_sv_gets’:

sv.c:4419: error: ‘FILE’ has no member named ‘_IO_read_end’

sv.c:4419: error: ‘FILE’ has no member named ‘_IO_read_ptr’

sv.c:4435: error: ‘FILE’ has no member named ‘_IO_read_ptr’

sv.c:4473: error: ‘FILE’ has no member named ‘_IO_read_ptr’

sv.c:4486: error: ‘FILE’ has no member named ‘_IO_read_end’

sv.c:4486: error: ‘FILE’ has no member named ‘_IO_read_ptr’

sv.c:4487: error: ‘FILE’ has no member named ‘_IO_read_ptr’

sv.c:4514: error: ‘FILE’ has no member named ‘_IO_read_ptr’

make[3]: *** [sv.o] Error 1

 

 

 

Any ideas?

 

 

 

Thanks in advance

 

 

 

Emanuele

TranslateQuoteReplyEditDelete

 

 

2009-02-06 11:56:38     Re: Compiling Perl..

Emanuele Italia (ITALY)

Message: 68996   

 

I installed the "microperl" (http://rowetel.com/ucasterisk/ipkg/Packages)  but it looks quite limited.

 

Do you have any suggestions how to compile a "normal" Perl?

 

 

 

Thanks

 

 

 

Emanuele

TranslateQuoteReplyEditDelete

 

 

2009-02-06 13:19:30     Re: Compiling Perl..

Mike Frysinger (UNITED STATES)

Message: 68999   

 

microperl is the only thing that cross-compiles.  if you want more (like the extended packages), you'll need to compile things yourself.

QuoteReplyEditDelete

 

 

2009-02-06 13:19:47     Re: Compiling Perl..

Mike Frysinger (UNITED STATES)

Message: 69000   

 

it's broken in the branch and has been fixed in trunk already

QuoteReplyEditDelete

 

 

2009-02-09 04:50:36     Re: Compiling Perl..

Emanuele Italia (ITALY)

Message: 69077   

 

It doesn't compile the Perl from trunk..but i just download the perl directory.

 

do i have to download all trunk tree?

 

Thanks in advance

 

 

 

Emanuele

TranslateQuoteReplyEditDelete

 

 

2009-02-09 11:55:23     Re: Compiling Perl..

Mike Frysinger (UNITED STATES)

Message: 69136   

 

i imagine it'd work just dropping it into the 2008R1.5 release, but we've never tested it and doing that isnt supported, so if it breaks ...

Attachments

    Outcomes