2009-02-03 03:19:18     Serial program to download file

Document created by Aaronwu Employee on Aug 11, 2013
Version 1Show Document
  • View in full screen mode

2009-02-03 03:19:18     Serial program to download file

V Hemanth Kumar (INDIA)

Message: 68701   

 

Hi,

 

Is there any application in the uClinux dist which can download a file through serial port (uart) (Example kermit or minicom)?

 

I am using the uClinux-dist-2008R1.5-RC3 release for BF527 ezkit.

 

~Hemanth

 

 

QuoteReplyEditDelete

 

 

2009-02-03 08:04:00     Re: Serial program to download file

Robin Getz (UNITED STATES)

Message: 68762   

 

Hemanth:

 

How about zmodem? (rz/sz) - picocom is also in the dist as a terminal application.

 

-Robin

QuoteReplyEditDelete

 

 

2009-02-03 11:33:41     Re: Serial program to download file

V Hemanth Kumar (INDIA)

Message: 68779   

 

Thanks Robin. Will try it and get back.

 

~Hemanth.V

QuoteReplyEditDelete

 

 

2009-02-06 03:38:16     Re: Serial program to download file

Izhar Eyal (ISRAEL)

Message: 68954   

 

We use lsz/lrz to send receive on serial on the target board, on the PC just use minicom CTRL+A, and choose S.

 

works just fine.

Attachments

    Outcomes