2009-02-04 15:44:58     Combination from kernel-2008R1.5 and userspace 2009pre

Document created by Aaronwu Employee on Aug 9, 2013
Version 1Show Document
  • View in full screen mode

2009-02-04 15:44:58     Combination from kernel-2008R1.5 and userspace 2009pre

Patrick Hotz (GERMANY)

Message: 68860   

 

Hi Guys,

 

I have a little question about the combination from kernel-2008R1.5 and the userspace from 2009pre...

 

For a programm we need the current uClinux-dist2008R1.5.

Our problem is that we also want to use some programms from 2009pre which are broken down in 2008R1.5.

 

My question is following...

if i copy the whole linux-folder from 2008R1.5 in the dist-2009pre folder, is the uClinux running ok?

I have tried it today and it seems to be working... the kernel 2008 boots and i can run programms from dist2009.

The "version" shows Kernel: 2008R1.5 and userspace pre-svn

 

Has anybody tried something else?

Is it save to do that?

 

 

 

- Patrick

TranslateQuoteReplyEditDelete

 

 

2009-02-04 15:47:24     Re: Combination from kernel-2008R1.5 and userspace 2009pre

Mike Frysinger (UNITED STATES)

Message: 68861   

 

running across versions really isnt supported ... better to fix said program to not need 2008R1.5

Attachments

    Outcomes