2009-02-02 10:20:27     _bfin_serial_console_putchar causes MPU violation?

Document created by Aaronwu Employee on Aug 9, 2013
Version 1Show Document
  • View in full screen mode

2009-02-02 10:20:27     _bfin_serial_console_putchar causes MPU violation?

Steve Strobel (UNITED STATES)

Message: 68678   

 

In an effort to track down some application software bugs, I turned on memory protection in my uClinux build. Near the end of the boot process (after /etc/rc prints the MOTD), it now continously stack dumps complaining of a "CPLB protection violation" with a stack track that goes back to _bfin_serial_console_putchar. Looking at the forum archives, it seems that others are using the memory protection, so I am wondering what I am doing wrong.

 

The hardware is a custom BF537 design similar to the BF537 stamp. The BF537 chip is rev 0.3. I am using a Linux release 2.6.22.19-ADI-2008R1.5-svn408, build #26 Mon Jan 26 15:30:47 MST 2009 with a few custom drivers.  A log of the serial messages printed on bootup follows:

 

## Booting image at 02000000 ...

   Image Name:   uClinux Kernel and ext2

   Created:      2009-01-28  21:32:35 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    7462436 Bytes =  7.1 MB

   Load Address: 00001000

   Entry Point:  001a6000

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 1a6000

Linux version 2.6.22.19-ADI-2008R1.5-svn408 (stevestrobel@dev1-ubuntu) (gcc version 4.1.2 (ADI svn)) #27 Wed Jan 28 13:3

9:17 MST 2009

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.3

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  text      = 0x00001000-0x0013b880

  rodata    = 0x0013c000-0x00191704

  data      = 0x00192000-0x001a6000

    stack   = 0x00192000-0x00194000

  init      = 0x001a6000-0x001b9000

  bss       = 0x001b9000-0x001c9b10

  available = 0x001c9b10-0x02000000

  rootfs    = 0x02000000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

MPU: setting up cplb tables with memory protection

Instruction Cache Enabled

Data Cache Enabled (write-back)

Built 1 zonelists.  Total pages: 8128

Kernel command line: root=/dev/mtdblock0 rw console=ttyBF0,115200

Configuring Blackfin Priority Driven Interrupts

Hardware Trace expanded to 2k

PID hash table entries: 128 (order: 7, 512 bytes)

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Memory available: 28376k/65536k RAM, (76k init code, 1258k kernel code, 492k data, 1024k dma, 2568k reserved)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (15 KB free)

Blackfin Data B SRAM: 16 KB (13 KB free)

Blackfin Instruction SRAM: 48 KB (40 KB free)

Security Framework v1.0.0 initialized

Capability LSM initialized

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

msat_ip_board_init(): registering device resources

msat_ip_board_init(): registering Blackfin SPI resources

msat_ip_board_init(): finished registering Blackfin SPI resources

Generic PHY: Registered new driver

SCSI subsystem initialized

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 1024 (order: 1, 8192 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 1024 bind 1024)

TCP reno registered

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

ISA-BlackFin-CAN CAN Driver 3.4.6_AD_BLACKFIN (c) Jan 28 2009

BlackFin port by H.J. Oertel (oe@port.de)

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

MSAT-IP leds driver

MSAT-IP ptts driver

MSAT-IP cors driver

RLC-DSP4 pls driver

RLC-DSP4 inputs driver

RLC-DSP4 outputs driver

RLC-DSP4 dtmf_data driver

RLC-DSP4 ltc1863_adc driver

ltc1863_spi_init

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 20) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac: Version 1.1, Blackfin BF53[67] BF527 on-chip Ethernet MAC driver

uclinux[mtd]: RAM probe address=0x2000000 size=0x1f00000

Creating 1 MTD partitions on "RAM":

0x00000000-0x01f00000 : "ROMfs"

m25p80 spi0.1: m25p128 (16384 Kbytes)

Creating 4 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader"

0x00040000-0x00080000 : "bootloader-environment"

0x00080000-0x00e00000 : "kernel"

0x00e00000-0x01000000 : "file system"

ltc1863_spi_probe with spi pointer 0x0058bb84

ltc1863_spi_probe: chip 0058aeac, spi 0058bb84

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Contoller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

bfin-spi-gpio-mstr: registering platform driver

bfin-spi-gpio-mstr: bfin_spi_gpio_probe()

bits_per_word not specified in spi_bitbang_setup.  Defaulting to 32.

bits_per_word not specified in spi_bitbang_setup.  Defaulting to 32.

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).

dma_alloc_init: dma_page @ 0x005a0000 - 256 pages at 0x03f00000

snd_ad1836_configure

ALSA device list:

  #0: ADI ad1836 at PF4 SPORT0 rx/tx dma 3/4 err irq 45

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

VFS: Mounted root (ext2 filesystem).

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

CPLB protection violation

- Illegal instruction fetch access (memory protection violation).

Defered Exception context

CURRENT PROCESS:

COMM=init PID=1

TEXT = 0x005c0000-0x005c2a00        DATA = 0x005bfa00-0x005bfe48

BSS = 0x005bfe48-0x005e0000  USER-STACK = 0x005fff00

 

return address: [0x0068e886]; contents of:

0x0068e860:  b0f2  3039  3017  63f8  300b  e300  0007  e801

0x0068e870:  0000  0538  0010  0000  0578  e800  0003  a1bb

0x0068e880:  e128  0072  00a0 [3038] e120  f000  0a07  1006

0x0068e890:  3007  e801  0000  0538  0010  e3ff  e8b2  3210

 

SEQUENCER STATUS:               Not tainted

SEQSTAT: 0000202b  IPEND: 0030  SYSCFG: 0006

  HWERRCAUSE: 0x0

  EXCAUSE   : 0x2b

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x00466000> /* unknown address */

RETX: <0x0068e886> [ /lib/libuClibc-0.9.29.so + 0xe886 ]

RETS: <0x0068e852> [ /lib/libuClibc-0.9.29.so + 0xe852 ]

PC  : <0x0068e886> [ /lib/libuClibc-0.9.29.so + 0xe886 ]

DCPLB_FAULT_ADDR: <0x001bb880> /* unknown address */

ICPLB_FAULT_ADDR: <0x0000e498> { _release_console_sem + 0x1c0 }

 

PROCESSOR STATE:

R0 : 00000077    R1 : 005ffd10    R2 : 00000000    R3 : 00000000

R4 : 005fff04    R5 : 005fff04    R6 : 00000001    R7 : 00000077

P0 : 00000072    P1 : 0068e840    P2 : 005d11f0    P3 : 006c1bd8

P4 : 006c3d94    P5 : 005bfdcc    FP : 005ffc60    SP : 00465f24

LB0: 005ce181    LT0: 005ce174    LC0: 00000000

LB1: 005ccec7    LT1: 005ccec6    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 005ffce9

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 006c1bd8

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 005ffc54  ASTAT: 02003025

 

Hardware Trace:

   0 Target : <0x000044a4> { _dump_bfin_trace_buffer + 0x0 }

     Source : <0x00004ae8> { _trap_c + 0x12c }

   1 Target : <0x00004ae8> { _trap_c + 0x12c }

     Source : <0x000044a0> { _show_regs + 0x394 }

   2 Target : <0x0000449a> { _show_regs + 0x38e }

     Source : <0x0000e0da> { _printk + 0x16 }

   3 Target : <0x0000e0d6> { _printk + 0x12 }

     Source : <0x0000df94> { _vprintk + 0x1c0 }

   4 Target : <0x0000df7a> { _vprintk + 0x1a6 }

     Source : <0x0000e4d6> { _release_console_sem + 0x1fe }

   5 Target : <0x0000e4d0> { _release_console_sem + 0x1f8 }

     Source : <0x0000ddb0> { _wake_up_klogd + 0x24 }

   6 Target : <0x0000dd8c> { _wake_up_klogd + 0x0 }

     Source : <0x0000e4cc> { _release_console_sem + 0x1f4 }

   7 Target : <0x0000e4c8> { _release_console_sem + 0x1f0 }

     Source : <0x0000e4ba> { _release_console_sem + 0x1e2 }

   8 Target : <0x0000e4b0> { _release_console_sem + 0x1d8 }

     Source : <0x0000e4a2> { _release_console_sem + 0x1ca }

   9 Target : <0x0000e358> { _release_console_sem + 0x80 }

     Source : <0x0000e326> { _release_console_sem + 0x4e }

  10 Target : <0x0000e464> { _release_console_sem + 0x18c }

     Source : <0x0000e45e> { _release_console_sem + 0x186 }

  11 Target : <0x0000dc68> { __call_console_drivers + 0x60 }

     Source : <0x0000dc62> { __call_console_drivers + 0x5a }

  12 Target : <0x0000dc42> { __call_console_drivers + 0x3a }

     Source : <0x0000dc32> { __call_console_drivers + 0x2a }

  13 Target : <0x0000dc22> { __call_console_drivers + 0x1a }

     Source : <0x0000dc08> { __call_console_drivers + 0x0 }

  14 Target : <0x0000e45a> { _release_console_sem + 0x182 }

     Source : <0x0000e450> { _release_console_sem + 0x178 }

  15 Target : <0x0000e3de> { _release_console_sem + 0x106 }

     Source : <0x0000e3d8> { _release_console_sem + 0x100 }

  16 Target : <0x0000dc68> { __call_console_drivers + 0x60 }

     Source : <0x0000dc62> { __call_console_drivers + 0x5a }

  17 Target : <0x0000dc06> { ___call_console_drivers + 0x52 }

     Source : <0x0000dbfa> { ___call_console_drivers + 0x46 }

  18 Target : <0x000b3eae> { _bfin_serial_console_write + 0x46 }

     Source : <0x000b3ea8> { _bfin_serial_console_write + 0x40 }

  19 Target : <0x000b3e9a> { _bfin_serial_console_write + 0x32 }

     Source : <0x000b3e96> { _bfin_serial_console_write + 0x2e }

  20 Target : <0x000b1b08> { _uart_console_write + 0x44 }

     Source : <0x000b1afe> { _uart_console_write + 0x3a }

  21 Target : <0x000b3e62> { _bfin_serial_console_putchar + 0x52 }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

  22 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

  23 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

 

[snip - the same two addresses repeat over and over]

 

262 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

263 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

264 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x0000e482> { _release_console_sem + 0x1aa }

Stack from 00465f00:

        00000000 005ffc60 ffa007c0 00196564 00196564 00196560 00000000 005fff04

        000b1876 0068e886 00000030 0000202b 00000000 00466000 0068e886 0068e886

        0068e852 00000077 02003025 005ccec7 005ce181 005ccec6 005ce174 00000000

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

        00000000 00000000 00000000 006c1bd8 005ffce9 005ffc54 005ffc60 005bfdcc

 

Call Trace:

 

CPLB protection violation

- Illegal instruction fetch access (memory protection violation).

Defered Exception context

CURRENT PROCESS:

COMM=init PID=1

TEXT = 0x005c0000-0x005c2a00        DATA = 0x005bfa00-0x005bfe48

BSS = 0x005bfe48-0x005e0000  USER-STACK = 0x005fff00

 

return address: [0x0068e886]; contents of:

0x0068e860:  b0f2  3039  3017  63f8  300b  e300  0007  e801

0x0068e870:  0000  0538  0010  0000  0578  e800  0003  a1bb

0x0068e880:  e128  0072  00a0 [3038] e120  f000  0a07  1006

0x0068e890:  3007  e801  0000  0538  0010  e3ff  e8b2  3210

 

SEQUENCER STATUS:               Not tainted

SEQSTAT: 0006202b  IPEND: 0030  SYSCFG: 0006

  HWERRCAUSE: 0x18

  EXCAUSE   : 0x2b

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x00466000> /* unknown address */

RETX: <0x0068e886> [ /lib/libuClibc-0.9.29.so + 0xe886 ]

RETS: <0x0068e852> [ /lib/libuClibc-0.9.29.so + 0xe852 ]

PC  : <0x0068e886> [ /lib/libuClibc-0.9.29.so + 0xe886 ]

DCPLB_FAULT_ADDR: <0x00196570> /* unknown address */

ICPLB_FAULT_ADDR: <0x0000e498> { _release_console_sem + 0x1c0 }

 

PROCESSOR STATE:

R0 : 00000077    R1 : 005ffd10    R2 : 00000000    R3 : 00000000

R4 : 005fff04    R5 : 005fff04    R6 : 00000001    R7 : 00000077

P0 : 00000072    P1 : 0068e840    P2 : 005d11f0    P3 : 006c1bd8

P4 : 006c3d94    P5 : 005bfdcc    FP : 005ffc60    SP : 00465f24

LB0: 005ce181    LT0: 005ce174    LC0: 00000000

LB1: 005ccec7    LT1: 005ccec6    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 005ffce9

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 006c1bd8

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 005ffc54  ASTAT: 02003025

 

Hardware Trace:

   0 Target : <0x000044a4> { _dump_bfin_trace_buffer + 0x0 }

     Source : <0x00004ae8> { _trap_c + 0x12c }

   1 Target : <0x00004ae8> { _trap_c + 0x12c }

     Source : <0x000044a0> { _show_regs + 0x394 }

   2 Target : <0x0000449a> { _show_regs + 0x38e }

     Source : <0x0000e0da> { _printk + 0x16 }

   3 Target : <0x0000e0d6> { _printk + 0x12 }

     Source : <0x0000df94> { _vprintk + 0x1c0 }

   4 Target : <0x0000df7a> { _vprintk + 0x1a6 }

     Source : <0x0000e4d6> { _release_console_sem + 0x1fe }

   5 Target : <0x0000e4d0> { _release_console_sem + 0x1f8 }

     Source : <0x0000ddb0> { _wake_up_klogd + 0x24 }

   6 Target : <0x0000dd8c> { _wake_up_klogd + 0x0 }

     Source : <0x0000e4cc> { _release_console_sem + 0x1f4 }

   7 Target : <0x0000e4c8> { _release_console_sem + 0x1f0 }

     Source : <0x0000e4ba> { _release_console_sem + 0x1e2 }

   8 Target : <0x0000e4b0> { _release_console_sem + 0x1d8 }

     Source : <0x0000e4a2> { _release_console_sem + 0x1ca }

   9 Target : <0x0000e358> { _release_console_sem + 0x80 }

     Source : <0x0000e326> { _release_console_sem + 0x4e }

  10 Target : <0x0000e464> { _release_console_sem + 0x18c }

     Source : <0x0000e45e> { _release_console_sem + 0x186 }

  11 Target : <0x0000dc68> { __call_console_drivers + 0x60 }

     Source : <0x0000dc62> { __call_console_drivers + 0x5a }

  12 Target : <0x0000dc42> { __call_console_drivers + 0x3a }

     Source : <0x0000dc32> { __call_console_drivers + 0x2a }

  13 Target : <0x0000dc22> { __call_console_drivers + 0x1a }

     Source : <0x0000dc08> { __call_console_drivers + 0x0 }

  14 Target : <0x0000e45a> { _release_console_sem + 0x182 }

     Source : <0x0000e450> { _release_console_sem + 0x178 }

  15 Target : <0x0000e3de> { _release_console_sem + 0x106 }

     Source : <0x0000e3d8> { _release_console_sem + 0x100 }

  16 Target : <0x0000dc68> { __call_console_drivers + 0x60 }

     Source : <0x0000dc62> { __call_console_drivers + 0x5a }

  17 Target : <0x0000dc06> { ___call_console_drivers + 0x52 }

     Source : <0x0000dbfa> { ___call_console_drivers + 0x46 }

  18 Target : <0x000b3eae> { _bfin_serial_console_write + 0x46 }

     Source : <0x000b3ea8> { _bfin_serial_console_write + 0x40 }

  19 Target : <0x000b3e9a> { _bfin_serial_console_write + 0x32 }

     Source : <0x000b3e96> { _bfin_serial_console_write + 0x2e }

  20 Target : <0x000b1b08> { _uart_console_write + 0x44 }

     Source : <0x000b1afe> { _uart_console_write + 0x3a }

  21 Target : <0x000b3e62> { _bfin_serial_console_putchar + 0x52 }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

  22 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

  23 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

 

[and it repeats forever]

 

Thanks for any suggestions,

 

Steve

 

P.S.  It seems that whenever there are two consecutive spaces like this "  " in a message on this forum that it displays as an A with a "hat" over it in my email program (Eudora). This is the only forum or mailing list (of dozens I have joined) that works that way.  Is there a chance that something isn't right with the forum software or configuration, or is it just my setup?

QuoteReplyEditDelete

 

 

2009-02-02 11:38:39     Re: _bfin_serial_console_putchar causes MPU violation?

Mike Frysinger (UNITED STATES)

Message: 68682   

 

that trace shows that printk() was called after the crash happened, so it's most likely meaningless

 

you can try using the option that extends the hardware trace buffer to more than 16 entries

QuoteReplyEditDelete

 

 

2009-02-02 11:58:35     Re: _bfin_serial_console_putchar causes MPU violation?

Steve Strobel (UNITED STATES)

Message: 68684   

 

That option is enabled, which is why it is printing 265 entries rather than just 16.  Entries 22 through 263 are identical (some of them snipped for brevity), as shown in the original log and repeated below.  Are you suggesting that I should extend the size of the trace buffer even more?

 

20 Target : <0x000b1b08> { _uart_console_write + 0x44 }

     Source : <0x000b1afe> { _uart_console_write + 0x3a }

  21 Target : <0x000b3e62> { _bfin_serial_console_putchar + 0x52 }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

  22 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

  23 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

 

[snip - the same two addresses repeat over and over]

 

262 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

263 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x000b3e36> { _bfin_serial_console_putchar + 0x26 }

264 Target : <0x000b3e4e> { _bfin_serial_console_putchar + 0x3e }

     Source : <0x0000e482> { _release_console_sem + 0x1aa }

 

Steve

QuoteReplyEditDelete

 

 

2009-02-02 12:08:30     Re: _bfin_serial_console_putchar causes MPU violation?

Mike Frysinger (UNITED STATES)

Message: 68685   

 

that just shows the console driver polling the status bit

 

are you using the latest 2008R1.5 svn branch ?  there have been many fixes to the MPU since the release

QuoteReplyEditDelete

 

 

2009-02-02 12:38:42     Re: _bfin_serial_console_putchar causes MPU violation?

Steve Strobel (UNITED STATES)

Message: 68687   

 

I appears from my notes that we are using uClinux-dist-2008R1.5-RC3.tar.bz2 with our drivers added.  I will just turn the MPU off until I get a chance to update to a later version of the distribution.  Thanks for your help.

 

Steve

QuoteReplyEditDelete

 

 

2009-02-02 13:14:58     Re: _bfin_serial_console_putchar causes MPU violation?

Mike Frysinger (UNITED STATES)

Message: 68689   

 

that's best ... the MPU worked at first blush in the latest release, but under more usage it fell apart.  that should all be fixed now in the latest svn branch though.

Attachments

    Outcomes