2009-01-26 12:45:48     Running user application on system startup

Document created by Aaronwu Employee on Aug 9, 2013
Version 1Show Document
  • View in full screen mode

2009-01-26 12:45:48     Running user application on system startup

Vasanth Nayak (INDIA)

Message: 68352   

 

Hi all,

 

             I wanted to know which file i need to modify(maybe in rc.d directory or inittab or something) and what do i need to add to make a user application run at system startup.

 

I got some information  from http://docs.blackfin.uclinux.org/doku.php?id=adding_user_applications about builiding and integrating the application into the kernel.But that did not give information on autorunning it on startup.

 

Thanks

 

Vasanth

 

 

QuoteReplyEditDelete

 

 

2009-01-26 13:14:27     Re: Running user application on system startup

Mike Frysinger (UNITED STATES)

Message: 68353   

 

you're free to do userspace startup however you want.  the default simpleinit runs /etc/rc.

Attachments

    Outcomes