2008-12-29 12:32:22     AD7877 doesn't work when setting bus_num=1

Document created by Aaronwu Employee on Aug 9, 2013
Version 1Show Document
  • View in full screen mode

2008-12-29 12:32:22     AD7877 doesn't work when setting bus_num=1

Jimmy Dullaert (BELGIUM)

Message: 67157   

 

Hi,

 

With the 2008r1.5 release the AD7877 doesn't  work when the AD7877 is set to bus_num=1. In release 2007 this does work correctly.

 

The board is BF537 ezkit and the AD7877 is connected to SPI1 and CS7

 

Best regards,

 

Jimmy

QuoteReplyEditDelete

 

 

2008-12-29 15:18:39     Re: AD7877 doesn't work when setting bus_num=1

Mike Frysinger (UNITED STATES)

Message: 67158   

 

the BF537 doesnt have a SPI1, so there's no way it is going to work.  it only has SPI0.

Attachments

    Outcomes