2008-12-09 10:06:56     Installing uClinux on BF537-STAMP with AD1836

Document created by Aaronwu Employee on Aug 9, 2013
Version 1Show Document
  • View in full screen mode

2008-12-09 10:06:56     Installing uClinux on BF537-STAMP with AD1836

Yuval Yosef (ISRAEL)

Message: 66569   

 

Hi,

 

I'm trying to install uClinux on a ADZS-BF537-STAMP board with  AD1836AZ Dauther board attached.

 

Tried to compile uClinux kernel with ALSA module but I don't see the module when I boot the stamp board.

 

According to the manuals, when the board boots we should see the following message:

 

------------------------------------------------------------------

 

Advance Linux Sound Arch. Driver Version.......

 

.....

 

ALSA device list:

 

#0: ADI ad1836 at PF4 SPORT0.........

 

---------------------------------------------------------------------

 

  there is no such message !!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!

 

 

 

When I enter the command "lsmod" I get the following modules:

 

"snd_pcm_oss, snd_mixer_oss, snd_ad1836, snd_pcm,snd_timer, snd_page_alloc, snd, soundcore."

 

 

 

I can execute "tone" command  (there is a tone...)

 

 

 

can anyone jelp me???

 

Thanks,

 

Yuval

QuoteReplyEditDelete

 

 

2008-12-09 10:11:06     Re: Installing uClinux on BF537-STAMP with AD1836

Mike Frysinger (UNITED STATES)

Message: 66571   

 

the new AD1836A revision (Z -- lead free) has not been tested ... it seems to not work

Attachments

    Outcomes