2008-12-06 03:26:30     dhcp problem

Document created by Aaronwu Employee on Aug 9, 2013
Version 1Show Document
  • View in full screen mode

2008-12-06 03:26:30     dhcp problem

andy (UNITED STATES)

Message: 66438   

 

Am using lantronix module as a wireless bridge with the blackfin. Upon running dhclient eth0 i get the follwing message:

 

Listening on LPF/eth0/02:80:ad:20:31:b8

Sending on LPF/eth0/02:80:ad:20:31:b8

Sending on Socket/fallback/fallback-net

 

DHCPDISCOVER on eth0 tp 255.255.255.255 port 67 interval 3

 

ip length 328 disagrees with bytes received 332.

 

accepting packet with data after udp payload.

 

DHCP offer from 128.237.224.3

 

execve (/etc/dhclient-script, ..): No such file or directory exiting.

 

ip length 328 disagrees with bytes received 332.

......

..

.

.

and it keeps repeating.

 

from the messages it is obvious that I do not have the dhclient-script. But I dont know if the error is caused because of that. Also  I installed dhclient by choosing it in menuconfig. Is that not supposed to have dhclient-script installed too? How do I get the dhclient to work properly?

 

 

QuoteReplyEditDelete

 

 

2008-12-06 03:38:11     Re: dhcp problem

Mike Frysinger (UNITED STATES)

Message: 66439   

 

why are you using dhclient rather than dhcpcd ?

QuoteReplyEditDelete

 

 

2008-12-06 09:25:12     Re: dhcp problem

andy (UNITED STATES)

Message: 66458   

 

when I do a dhcpcd eth0 nothing happens. Infact it does not even complete and the prompt never comes back.

QuoteReplyEditDelete

 

 

2008-12-06 12:17:58     Re: dhcp problem

andy (UNITED STATES)

Message: 66459   

 

sorry..take back my statement. dhcpcd corrected the problem. thanks.

Attachments

    Outcomes