2008-12-04 03:59:10     bool type

Document created by Aaronwu Employee on Aug 9, 2013
Version 1Show Document
  • View in full screen mode

2008-12-04 03:59:10     bool type

vijai ragavan (INDIA)

Message: 66276   

 

Hai,

 

I am working on 2008R1. In this, bool type is not supported.Is there any header file(for supporting bool) to include in the project?

QuoteReplyEditDelete

 

 

2008-12-04 04:06:47     Re: bool type

Mike Frysinger (UNITED STATES)

Message: 66277   

 

bool type works just fine and always has.  you probably didnt include stdbool.h.

QuoteReplyEditDelete

 

 

2008-12-04 04:33:35     Re: bool type

vijai ragavan (INDIA)

Message: 66335   

 

hai,

 

Please send me the path for that file on 2008R1

QuoteReplyEditDelete

 

 

2008-12-04 04:37:06     Re: bool type

Mike Frysinger (UNITED STATES)

Message: 66336   

 

it's part of the toolchain

QuoteReplyEditDelete

 

 

2008-12-04 05:01:20     Re: bool type

vijai ragavan (INDIA)

Message: 66339   

 

can I include the header file in my project?

QuoteReplyEditDelete

 

 

2008-12-04 07:20:14     Re: bool type

Robin Getz (UNITED STATES)

Message: 66349   

 

vijai:

 

That is what Mike said to do - use stdbool.h

 

-Robin

Attachments

    Outcomes