2008-11-27 16:33:52     ooh323c channel driver for asterisk on IP04

Document created by Aaronwu Employee on Aug 9, 2013
Version 1Show Document
  • View in full screen mode

2008-11-27 16:33:52     ooh323c channel driver for asterisk on IP04

Tihomir Culjaga (CROATIA)

Message: 65924   

 

Hello,

 

i'm trying to compile ooh323c channel driver for asterisk planed to be running on an IP04 box. I still need help... Please!

 

I'm using the baps trunk from astfin.org:

 

svn co http://svn.astfin.org/software/baps/trunk baps

 

and a 2007R1.1_RC3 blackfin toolchain

 

http://blackfin.uclinux.org/gf/download/frsrelease/348/3347/blackfin-toolchain-07r1.1-3.i386.tar.gz

 

Of course I'm able to compile uClinux-dist and upload a working image to the IP04.

 

After asterisk-1.4.4 compiled, i tried with ooh323c from asterisk-addon (e.g. 1.4.4) but it doesn't work!

 

 

baps is located in: /home/tculjaga/BAPs/baps/

 

asterisk-1.4.4 is located in: /home/tculjaga/BAPs/baps/asterisk-1.4.4/

 

ooh323c is located in: /home/tculjaga/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$

 

 

I tried to configure ooh323 like this:

 

 

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$ ./configure --host=bfin-linux-uclibc --disable-largefile --without-pwlib --without-curl CFLAGS="-g -mfdpic -mfast-fp -ffast-math -D__FIXED_PT__ -D__BLACKFIN__ -Ibaps/uClinux-dist/staging/usr/include -fno-jump-tables" LDFLAGS="-mfdpic -Lbaps/uClinux-dist/staging/usr/lib -lpthread -ldl"

configure: WARNING: If you wanted to set the --build type, don't use --host.

    If a cross compiler is detected then cross compile mode will be used.

checking for a BSD-compatible install... /usr/bin/install -c

checking whether build environment is sane... yes

checking for gawk... no

checking for mawk... mawk

checking whether make sets $(MAKE)... yes

checking for bfin-linux-uclibc-strip... bfin-linux-uclibc-strip

checking for bfin-linux-uclibc-gcc... bfin-linux-uclibc-gcc

checking for C compiler default output file name... a.out

checking whether the C compiler works... yes

checking whether we are cross compiling... yes

checking for suffix of executables...

checking for suffix of object files... o

checking whether we are using the GNU C compiler... yes

checking whether bfin-linux-uclibc-gcc accepts -g... yes

checking for bfin-linux-uclibc-gcc option to accept ISO C89... none needed

checking for style of include used by make... GNU

checking dependency style of bfin-linux-uclibc-gcc... gcc3

checking build system type... i686-pc-linux-gnu

checking host system type... Invalid configuration `bfin-linux-uclibc': machine `bfin-linux' not recognized

configure: error: /bin/sh config/config.sub bfin-linux-uclibc failed

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$

 

 

well, here i found that config.sub from ooh323c is doesn't know what to do with blackfin host!

 

Maybe i did it stupid, but i got a copy of config.sub from /home/tculjaga/BAPs/baps/asterisk-1.4.4/ and tried to configure again... and configure worked! Also, i added some path to asterisk include files ... just to be sure!

 

 

./configure --host=bfin-linux-uclibc --disable-largefile --without-pwlib --without-curl CFLAGS="-g -mfdpic -mfast-fp -ffast-math -D__FIXED_PT__ -D__BLACKFIN__ -I/home/tculjaga/BAPs/baps/uClinux-dist/staging/usr/include: -Isrc/ -I/home/tculjaga/BAPs/baps/asterisk-1.4.4/include -fno-jump-tables" LDFLAGS="-mfdpic -L/home/tculjaga/BAPs/baps/uClinux-dist/staging/usr/lib -lpthread -ldl"

 

 

After configure went well, i need to issue make... well here i spent a lot of time fixing include paths within asterisk source (home/tculjaga/BAPs/baps/asterisk-1.4.4/include) files.

 

Finally, make didn't complain about missing files and it went till the end... except one thing! I'm missing the the libchan_h323.so.1.0.1 module! it never gets build!

 

What make does is to generate files under .lib/ directory:

 

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$ ls -la .libs/

total 2084

drwxr-xr-x 2 tculjaga tculjaga    4096 2008-11-27 15:24 .

drwxr-xr-x 7 tculjaga tculjaga    4096 2008-11-27 15:24 ..

-rw-r--r-- 1 tculjaga tculjaga 2115668 2008-11-27 15:24 libchan_h323.a

lrwxrwxrwx 1 tculjaga tculjaga      18 2008-11-27 15:24 libchan_h323.la -> ../libchan_h323.la

-rw-r--r-- 1 tculjaga tculjaga     818 2008-11-27 15:24 libchan_h323.lai

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$

 

 

Well, after a while digging into output generated by make i come out with this:

 

 

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$ /bin/sh ./libtool --mode=link bfin-linux-uclibc-gcc   -DGNU -D_GNU_SOURCE -D_REENTRANT -D_COMPACT  -mfdpic -L/home/tculjaga/BAPs/baps/uClinux-dist/staging/usr/lib -lpthread -ldl -o libchan_h323.so -rpath /usr/local/lib -L./ooh323c/src -version-info 1:1:0 chan_h323.lo ooh323cDriver.lo ooCmdChannel.lo ooLogChan.lo ooUtils.lo ooGkClient.lo context.lo ooDateTime.lo decode.lo dlist.lo encode.lo errmgmt.lo memheap.lo ootrace.lo oochannels.lo ooh245.lo ooports.lo ooq931.lo ooCapability.lo ooSocket.lo perutil.lo eventHandler.lo ooCalls.lo ooStackCmds.lo ooh323.lo ooh323ep.lo printHandler.lo rtctype.lo ooTimer.lo H235-SECURITY-MESSAGESDec.lo H235-SECURITY-MESSAGESEnc.lo H323-MESSAGES.lo H323-MESSAGESDec.lo H323-MESSAGESEnc.lo MULTIMEDIA-SYSTEM-CONTROL.lo MULTIMEDIA-SYSTEM-CONTROLDec.lo MULTIMEDIA-SYSTEM-CONTROLEnc.lo -lpthread -shared

libtool: link: warning: `-version-info' is ignored for programs

bfin-linux-uclibc-gcc -DGNU -D_GNU_SOURCE -D_REENTRANT -D_COMPACT -mfdpic -o libchan_h323.so chan_h323.o ooh323cDriver.o ooCmdChannel.o ooLogChan.o ooUtils.o ooGkClient.o context.o ooDateTime.o decode.o dlist.o encode.o errmgmt.o memheap.o ootrace.o oochannels.o ooh245.o ooports.o ooq931.o ooCapability.o ooSocket.o perutil.o eventHandler.o ooCalls.o ooStackCmds.o ooh323.o ooh323ep.o printHandler.o rtctype.o ooTimer.o H235-SECURITY-MESSAGESDec.o H235-SECURITY-MESSAGESEnc.o H323-MESSAGES.o H323-MESSAGESDec.o H323-MESSAGESEnc.o MULTIMEDIA-SYSTEM-CONTROL.o MULTIMEDIA-SYSTEM-CONTROLDec.o MULTIMEDIA-SYSTEM-CONTROLEnc.o -shared  -L/home/tculjaga/BAPs/baps/uClinux-dist/staging/usr/lib -ldl -L/home/tculjaga/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c/ooh323c/src -lpthread  -Wl,--rpath -Wl,/usr/local/lib

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$

 

 

I generate the needed libchan_h323.so module ... ok it is not in .lib/ directory but it is still there:

 

 

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$ ls -la libchan_h323.so

-rwxr-xr-x 1 tculjaga tculjaga 1769171 2008-11-27 23:06 libchan_h323.so

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$

 

 

Happy with the file, I copy that to the IP04, restart asterisk and it thrown an error:

 

asterisk: can't resolve symbol '_rpl_malloc'

 

 

What did i wrong?

 

Can someone help?

 

 

 

 

 

ooh323c_config&build_info.rar

QuoteReplyEditDelete

 

 

2008-11-27 21:00:17     Re: ooh323c channel driver for asterisk on IP04

Mike Frysinger (UNITED STATES)

Message: 65928   

 

if you want shared libraries, then force the shared configure option.  if it still doesnt detect shared support, then you probably need to rebuild the autotool code.

 

configure tried to replace malloc() with rpl_malloc().  force the configure tests.  see vendors/config/bfin/config.site in current trunk.

QuoteReplyEditDelete

 

 

2008-11-28 03:16:05     Re: ooh323c channel driver for asterisk on IP04

Tihomir Culjaga (CROATIA)

Message: 65942   

 

Hi Mike,

 

 

 

Thanks for your answer... however i still cannot guess what my configure options should be.

 

 

 

I've checked vendors/config/bfin/* and all i can find is config.arch ... i guess thats it... but still

 

 

 

./configure --host=bfin-linux-uclibc --disable-largefile --without-pwlib --without-curl CFLAGS="-g -mfdpic -mfast-fp -ffast-math -D__FIXED_PT__ -D__BLACKFIN__ -I/home/tculjaga/BAPs/baps/uClinux-dist/staging/usr/include: -Isrc/ -I/home/tculjaga/BAPs/baps/asterisk-1.4.4/include -fno-jump-tables" LDFLAGS="-mfdpic -L/home/tculjaga/BAPs/baps/uClinux-dist/staging/usr/lib -lpthread -ldl"

 

pls, can you suggest the configure options?

 

 

QuoteReplyEditDelete

 

 

2008-11-28 04:14:47     Re: ooh323c channel driver for asterisk on IP04

Mike Frysinger (UNITED STATES)

Message: 65946   

 

as i said, look at current svn trunk, not the 2007R1 release

QuoteReplyEditDelete

 

 

2008-11-28 06:25:09     Re: ooh323c channel driver for asterisk on IP04

Mark T (UNITED STATES)

Message: 65955   

 

Tihomir,

 

I will be adding h323 support to Astfin2 trunk sometimes soon. Please contact me directly if you wish to help

 

Thanks,

 

Mark

QuoteReplyEditDelete

 

 

2008-12-03 08:12:39     Re: ooh323c channel driver for asterisk on IP04

Tihomir Culjaga (CROATIA)

Message: 66237   

 

Hi Mike,

 

 

 

thanks fro your response, i tried with config.site you suggested but it is not working

 

CONFIG_SITE=/path/to/config.site

 

./configure ...

 

Also, i've changed the configure script to enable shared libraries and now the .so module is build

 

line 7062 in attached configure script: linux-gnu* | linux-uclibc*)

 

 

 

 

./configure --host=bfin-linux-uclibc --enable-shared --disable-largefile --without-pwlib --without-curl \

                CFLAGS="-g -mfdpic -mfast-fp -ffast-math -D__FIXED_PT__ -D__BLACKFIN__ \

                -I/home/tculjaga/BAPs/baps/

uClinux-dist/staging/usr/include -Isrc/ \

                -I/home/tculjaga/BAPs/baps/asterisk-1.4.4/include -fno-jump-tables" \

                LDFLAGS="-mfdpic -L/home/tculjaga/BAPs/baps/uClinux-dist/staging/usr/lib \

                -lpthread -ldl -shared"

 

OPTIMIZE="-Os" ASTCFLAGS="-g -mfdpic -mfast-fp -ffast-math -D__FIXED_PT__ -D__BLACKFIN__ \

                  -I/home/tculjaga/BAPs/baps/uClinux-dist/staging/usr/include -fno-jump-tables" ASTLDFLAGS="-mfdpic \

                  -L/home/tculjaga/BAPs/baps/uClinux-dist/staging/usr/lib -lpthread -ldl" make -C \

                   /home/tculjaga/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c NOISY_BUILD=1

 

 

finnaly i got the module compiled:

 

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$ ls -la .libs/

total 3816

drwxr-xr-x 2 tculjaga tculjaga    4096 2008-12-03 14:35 .

drwxr-xr-x 7 tculjaga tculjaga    4096 2008-12-03 14:35 ..

-rw-r--r-- 1 tculjaga tculjaga 2115668 2008-12-03 14:35 libchan_h323.a

lrwxrwxrwx 1 tculjaga tculjaga      18 2008-12-03 14:35 libchan_h323.la -> ../libchan_h323.la

-rw-r--r-- 1 tculjaga tculjaga     890 2008-12-03 14:35 libchan_h323.lai

lrwxrwxrwx 1 tculjaga tculjaga      21 2008-12-03 14:35 libchan_h323.so -> libchan_h323.so.1.0.1

lrwxrwxrwx 1 tculjaga tculjaga      21 2008-12-03 14:35 libchan_h323.so.1 -> libchan_h323.so.1.0.1

-rwxr-xr-x 1 tculjaga tculjaga 1768680 2008-12-03 14:35 libchan_h323.so.1.0.1

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$

 

 

but still, the same issue ... when i run asterisk:

 

asterisk: can't resolve symbol '_rpl_malloc'

 

 

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$ strings .libs/libchan_h323.so.1.0.1 | grep malloc

_rpl_malloc

_g_malloc_func

tculjaga@subZero:~/BAPs/baps/asterisk-addons-1.4.4/asterisk-ooh323c$

 

It is still the configre not going well ...

 

 

 

any hint ?

 

configure

QuoteReplyEditDelete

 

 

2008-12-03 19:23:51     Re: ooh323c channel driver for asterisk on IP04

Mike Frysinger (UNITED STATES)

Message: 66266   

 

you have to find the malloc related tests in the configure script and make sure they're being set to the correct value.  often times cross-compile tests in configure assume the target malloc is broken and so force a rename to gnulib's rpl_malloc.

Outcomes