2008-11-20 18:03:07     Mouse BF537 UART1

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-11-20 18:03:07     Mouse BF537 UART1

damien OLLIVE (UNITED STATES)

Message: 65634   

 

Hy,

 

I work on BF537, i have a TFT-LCD connected to the board by PPI and i creat the PPI clock by the TIMER1

 

I have some issue about the toush screen with my customer that why i want to add a mouse to the board to continu to develop my application.

 

for information i develop application with QT4 opensource witch is embedded in blackfin and running well.

 

 

 

i have a USB mouse and i have built an adaptator for the Uart1 port of the blackfin 537 stamp board (with a max 232).

 

i have crosses the RX and TX signal put 5V in the RTS pin.

 

i have put 3 and 4 of SW5 to ON (1 and 2 OFF)

 

 

 

when i try this

 

stty -F /dev/ttyS1 ispeed 1200 cs7 -icanon

 

the kernel bug and don't respond to anything, i have to reboot the board.

 

 

 

cat /dev/ttyS1

 

elsif i haven't the file ttyS1

 

 

 

how can i do to enable a mouse or where can i found information about that please

 

 

 

thanks  Damien

QuoteReplyEditDelete

 

 

2008-11-20 18:26:07     Re: Mouse BF537 UART1

Mike Frysinger (UNITED STATES)

Message: 65635   

 

if you're trying to talk to the Blackfin UART1, why are you using /dev/ttyS1 ?  the Blackfin UARTs are /dev/ttyBF# ...

QuoteReplyEditDelete

 

 

2008-11-20 19:33:20     Re: Mouse BF537 UART1

damien OLLIVE (UNITED STATES)

Message: 65637   

 

hy mike,

 

i have tried to follow this idea :

 

http://docs.blackfin.uclinux.org/doku.php?id=setup_serial_mouse

 

I thinked that was writting (say me if i am wrong) that i can plug a mouse in the UART1 port and without kernel configuration, i can add a mouse with a command like that

 

stty -F /dev/ttyS1 ispeed 1200 cs7 -icanon

 

but my problem is i haven't the file ttyS1 or ttyFB1.

 

how configure linux to get it?

 

have i to configure the port P_UART1_RX and P_UART1_TX?

 

that could be and hardware problem or it's my linux configuration?

 

thanks for the help

QuoteReplyEditDelete

 

 

2008-11-20 19:41:54     Re: Mouse BF537 UART1

Mike Frysinger (UNITED STATES)

Message: 65639   

 

that is an example.  the assumption is you've properly configured your system and you substitue /dev/ttyS1 with the actual UART your mouse is connected to.

 

like i said already, if you're using the Blackfin UART, then the correct device node is /dev/ttyBF1.

Attachments

    Outcomes