2008-11-18 06:51:26     Booting error

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-11-18 06:51:26     Booting error

vijai ragavan (INDIA)

Message: 65437   

 

Hi,

 

the following error displayed when i run the application . Please suggest.

 

Jump to address 0 - 0x0fff

 

CURRENT PROCESS:

 

COMM=Philips_NP PID=81

TEXT = 0x00a82000-0x00c778b8  DATA = 0x00c828b8-0x019154a0

BSS = 0x019154a0-0x0069e000   USER-STACK = 0x006bdeb0

 

return address: 0x00000420; contents of [PC-16...PC+8]:

 

 

RETE:  00000000  RETN: 0061c000  RETX: 00000420  RETS: 00a356d8

IPEND: 0030  SYSCFG: 0036

SEQSTAT: 0000002d    SP: 0061bf24

R0: 00649010    R1: 00000000    R2: 00000001    R3: 00000001

R4: 00000000    R5: 006bf9c8    R6: 006c5380    R7: 00649000

P0: 00649010    P1: 00000000    P2: 00000420    P3: 006c5380

P4: 00000000    P5: 00649010    FP: 006bd9e4

A0.w: 00000000    A0.x: 00000000    A1.w: 00000000    A1.x: 00000000

LB0: 0043077d  LT0: 00430770  LC0: 00000000

LB1: 006061a3  LT1: 006061a2  LC1: 00000000

B0: 00000000  L0: 00000000  M0: 00000000  I0: 006bd9e5

B1: 00000000  L1: 00000000  M1: 00000000  I1: 00001000

B2: 00000000  L2: 00000000  M2: 00000000  I2: 00000000

B3: 00000000  L3: 00000000  M3: 00000000  I3: 00000000

 

USP: 006bd9d8   ASTAT: 02003025

DCPLB_FAULT_ADDR=00649010

ICPLB_FAULT_ADDR=00000420

 

 

Hardware Trace:

0 Target : <0x0018368c> { _trap_c + 0x0 }

   Source : <0xffa00b80> { _exception_to_level5 + 0xb4 }

1 Target : <0xffa00acc> { _exception_to_level5 + 0x0 }

   Source : <0xffa00aca> { _ex_trap_c + 0x5a }

2 Target : <0xffa00bf8> { _trap + 0x0 }

   Source : <0x00a356d6> [ /lib/libpthread-0.9.29.so + 0x76d6 ]

3 Target : <0x00a356b8> [ /lib/libpthread-0.9.29.so + 0x76b8 ]

   Source : <0x0043073e> [ /lib/ld-uClibc-0.9.29.so + 0x473e ]

4 Target : <0x0043072c> [ /lib/ld-uClibc-0.9.29.so + 0x472c ]

   Source : <0x0042e79e> [ /lib/ld-uClibc-0.9.29.so + 0x279e ]

5 Target : <0x0042e792> [ /lib/ld-uClibc-0.9.29.so + 0x2792 ]

   Source : <0x0042e75a> [ /lib/ld-uClibc-0.9.29.so + 0x275a ]

6 Target : <0x0042e74c> [ /lib/ld-uClibc-0.9.29.so + 0x274c ]

   Source : <0x0042e714> [ /lib/ld-uClibc-0.9.29.so + 0x2714 ]

7 Target : <0x0042e710> [ /lib/ld-uClibc-0.9.29.so + 0x2710 ]

   Source : <0x0042d20a> [ /lib/ld-uClibc-0.9.29.so + 0x120a ]

8 Target : <0x0042d204> [ /lib/ld-uClibc-0.9.29.so + 0x1204 ]

   Source : <0x0042d1e8> [ /lib/ld-uClibc-0.9.29.so + 0x11e8 ]

9 Target : <0x0042d1e4> [ /lib/ld-uClibc-0.9.29.so + 0x11e4 ]

   Source : <0x0042d1d6> [ /lib/ld-uClibc-0.9.29.so + 0x11d6 ]

10 Target : <0x0042d1ce> [ /lib/ld-uClibc-0.9.29.so + 0x11ce ]

   Source : <0x0042d200> [ /lib/ld-uClibc-0.9.29.so + 0x1200 ]

11 Target : <0x0042d1ec> [ /lib/ld-uClibc-0.9.29.so + 0x11ec ]

   Source : <0x0042d1cc> [ /lib/ld-uClibc-0.9.29.so + 0x11cc ]

12 Target : <0x0042d1c0> [ /lib/ld-uClibc-0.9.29.so + 0x11c0 ]

   Source : <0x0042e3e4> [ /lib/ld-uClibc-0.9.29.so + 0x23e4 ]

13 Target : <0x0042e3d8> [ /lib/ld-uClibc-0.9.29.so + 0x23d8 ]

   Source : <0x0042e3b2> [ /lib/ld-uClibc-0.9.29.so + 0x23b2 ]

14 Target : <0x0042e39a> [ /lib/ld-uClibc-0.9.29.so + 0x239a ]

   Source : <0x0042e380> [ /lib/ld-uClibc-0.9.29.so + 0x2380 ]

15 Target : <0x0042e366> [ /lib/ld-uClibc-0.9.29.so + 0x2366 ]

   Source : <0x0042e32e> [ /lib/ld-uClibc-0.9.29.so + 0x232e ]

Stack from 0061bf04:

        00000110 ffa00b84 002b46fc 002b46fc 002b46f8 006bd9d4 00000000 005190d2

        00000420 00000030 0000002d 00000000 0061c000 00000420 00000420 00a356d8

        00649010 02003025 006061a3 0043077d 006061a2 00430770 00000000 00000000

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

        00000000 00000000 00001000 006bd9e5 006bd9d8 006bd9e4 00649010 00000000

Call Trace:

 

SIGSEGV

QuoteReplyEditDelete

 

 

2008-11-18 08:46:58     Re: Booting error

Mike Frysinger (UNITED STATES)

Message: 65441   

 

please review this:

http://docs.blackfin.uclinux.org/doku.php?id=debuging_applications#analyzing_traces

Attachments

    Outcomes