2008-11-13 10:10:37     SMC driver issue

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-11-13 10:10:37     SMC driver issue

vijai ragavan (INDIA)

Message: 65243   

 

hi,

 

i am using 2007R1 distibution.The following error are displayed when i enable the SMC91x driver.Please suggest.

 

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 35) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

smc91x: IOADDR 2e000600 doesn't match configuration (7c0).

smc91x: IO 2e000600: Unrecognized revision register 0x3307, Contact author.

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth%d: timeout drivers/net/smc91x.c line 402

eth0: <NULL> (rev 7) at 2e000600 IRQ 82 [nowait]

eth0: Ethernet addr: ba:9d:08:41:c8:38

QuoteReplyEditDelete

 

 

2008-11-13 10:26:00     Re: SMC driver issue

Mike Frysinger (UNITED STATES)

Message: 65245   

 

please fully describe your hardware / software

 

QuoteReplyEditDelete

 

 

2008-11-13 23:48:51     Re: SMC driver issue

vijai ragavan (INDIA)

Message: 65262   

 

i am using bf561 custom board.

 

ethernernet chip name:LAN91c111

Attachments

    Outcomes