2008-11-12 10:04:59     could not mount usb on bf548

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-11-12 10:04:59     could not mount usb on bf548

Maha lakshmi (INDIA)

Message: 65162   

 

Hi,

 

   I have configured kernel with necessary things and it's detecting the usb.  but I could not mount it.

 

Please find the attached kernel bootup logs.

 

I connect the following msg when i connect to the usb.

 

usb 1-1: new high speed USB device using musb_hdrc and address 3

usb 1-1: Product: U3 Cruzer Micro

usb 1-1: Manufacturer: SanDisk Corporation

usb 1-1: SerialNumber: 0000161CB2755DB9

usb 1-1: configuration #1 chosen from 1 choice

 

 

but It's saying where to mount.

 

 

 

Thanks,

 

Maha

 

 

 

 

 

bfin> bootelf 0x1000000

Loading .text @ 0x00001000 (1688720 bytes)

Loading .rodata @ 0x0019e000 (450312 bytes)

Loading __ksymtab @ 0x0020bf08 (17544 bytes)

Loading __ksymtab_gpl @ 0x00210390 (5552 bytes)

Loading __ksymtab_gpl_future @ 0x00211940 (24 bytes)

Loading __ksymtab_strings @ 0x00211958 (56856 bytes)

Loading __param @ 0x0021f770 (1420 bytes)

Loading .data @ 0x00220000 (106496 bytes)

Loading .init.text @ 0x0023a000 (133496 bytes)

Loading .init.data @ 0x0025a978 (13092 bytes)

Loading .init.setup @ 0x0025dc9c (616 bytes)

Loading .initcall.init @ 0x0025df04 (600 bytes)

Loading .con_initcall.init @ 0x0025e15c (8 bytes)

Loading .init.ramfs @ 0x0025e164 (4844749 bytes)

Loading .text_l1 @ 0xffa00000 (5752 bytes)

sh_addr: FFA00000, p_paddr: 006FCE31

Loading from: 016FD000 to 006FCE31, size: 5752

Loading .data_l1 @ 0xff800000 (192 bytes)

sh_addr: FF800000, p_paddr: 006FE4A9

Loading from: 016FF000 to 006FE4A9, size: 192

Clearing .bss @ 0x006ff000 (87024 bytes)

## Starting application at 0x0023a000 ...

Linux version 2.6.22.18-ADI-2008R1-svn (root@localhost.localdomain) (gcc version 4.1.2 (ADI svn)) #29 Wed Nov 12 19:35:44 IS8early printk enabled on early_BFuart0

Hardware Trace Active and Enabled

Blackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF548 Rev 0.0

Warning: Compiled for Rev 0, but running on Rev 1

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  text      = 0x00001000-0x0019d490

  rodata    = 0x0019e000-0x0021fcfc

  data      = 0x00220000-0x0023a000

    stack   = 0x00220000-0x00222000

  init      = 0x0023a000-0x006ff000

  bss       = 0x006ff000-0x007143f0

  available = 0x007143f0-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists.  Total pages: 15748

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart1,57600 console=ttyBF0,57600

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

Console: colour dummy device 80x25

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 55652k/65536k RAM, (4884k init code, 1649k kernel code, 711k data, 2048k dma, 588k reserved)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (15 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 48 KB (42 KB free)

Security Framework v1.0.0 initialized

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, ?dma?, host, debug=0

musb_hdrc: kernel must blacklist external hubs

musb_hdrc: USB Host mode controller at ffc03c00 using PIO, IRQ 82

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: Product: MUSB HDRC host driver

usb usb1: Manufacturer: Linux 2.6.22.18-ADI-2008R1-svn musb-hcd

usb usb1: SerialNumber: musb_hdrc.0

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bf54x-lq043: FrameBuffer initializing...

dma_alloc_init: dma_page @ 0x03521000 - 512 pages at 0x03e00000

Console: switching to colour frame buffer device 80x24

bfin-otp: initialized

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 48) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

smsc911x: Driver version 2007-07-13.

register bfin atapi driver

scsi0 : pata-bf54x

ata1: PATA max UDMA/66 cmd 0x00000000 ctl 0xffc03800 bmdma 0x00000000 irq 68

ata1.00: ATA-6: TOSHIBA MK4032GAX, AD101A, max UDMA/100

ata1.00: 78140160 sectors, multi 16: LBA48

ata1.00: configured for UDMA/66

blk_queue_max_hw_segments: set to minimum 1

scsi 0:0:0:0: Direct-Access     ATA      TOSHIBA MK4032GA AD10 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 78140160 512-byte hardware sectors (40008 MB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sd 0:0:0:0: [sda] 78140160 512-byte hardware sectors (40008 MB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sda: sda1

sd 0:0:0:0: [sda] Attached SCSI disk

physmap platform flash device: 00400000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

NOR chip too large to fit in mapping. Attempting to cope...

Intel/Sharp Extended Query Table at 0x010A

  Unknown Intel/Sharp Extended Query version 1.5.

gen_probe: No supported Vendor Command Set found

physmap-flash physmap-flash.0: map_probe failed

BF5xx on-chip NAND FLash Controller Driver, Version 1.2 (c) 2007 Analog Devices, Inc.

bf5xx-nand bf5xx-nand.0: page_size=256, data_width=8, wr_dly=3, rd_dly=3

NAND device: Manufacturer ID: 0x20, Chip ID: 0xda (ST Micro NAND 256MiB 3,3V 8-bit)

Creating 2 MTD partitions on "NAND 256MiB 3,3V 8-bit":

0x00000000-0x00400000 : "Linux Kernel"

0x00400000-0x10000000 : "File System"

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Contoller Driver, Version 1.0, regs_base@ffc00500, dma channel@4

bfin-spi bfin-spi.1: Blackfin BF5xx on-chip SPI Contoller Driver, Version 1.0, regs_base@ffc02300, dma channel@5

sl811: driver sl811-hcd, 19 May 2005

input: bf54x-keys as /class/input/input0

bf54x-keys: Blackfin BF54x Keypad registered IRQ 76

ad7877 spi0.2: touchscreen, irq 123

input: AD7877 Touchscreen as /class/input/input1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

i2c-bfin-twi i2c-bfin-twi.1: Blackfin BF5xx on-chip I2C TWI Contoller Driver, Version 1.8, regs_base@ffc02200

usb 1-1: new high speed USB device using musb_hdrc and address 2

usb 1-1: Product: U3 Cruzer Micro

usb 1-1: Manufacturer: SanDisk Corporation

usb 1-1: SerialNumber: 0000161CB2755DB9

usb 1-1: configuration #1 chosen from 1 choice

usbcore: registered new interface driver usbhid

drivers/hid/usbhid/hid-core.c: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).

ASoC version 0.13.1

AD1980 SoC Audio Codec

asoc: AC97 <-> bf5xx-ac97 mapping ok

ALSA device list:

  #0: bf5xx-board (AD1980)

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting the system clock to 1970-01-12 00:21:57 (951717)

Freeing unused kernel memory: 4884k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.4.1 (2008-11-11 13:07:27 IST) Built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

 

bootlogs.doc

QuoteReplyEditDelete

 

 

2008-11-12 10:25:15     Re: could not mount usb on bf548

Mike Frysinger (UNITED STATES)

Message: 65163   

 

please stop posting MS Word files.  just post the log into your message.

QuoteReplyEditDelete

 

 

2008-11-12 10:26:15     Re: could not mount usb on bf548

Mike Frysinger (UNITED STATES)

Message: 65164   

 

did you enable usb mass storage support in your kernel ?

QuoteReplyEditDelete

Attachments

Outcomes