2008-11-10 09:18:29     trunk platform nand driver

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-11-10 09:18:29     trunk platform nand driver

Andras Szemzo (HUNGARY)

Message: 64935   

 

hi,

 

 

 

Is there a known build error with enabled platform nand driver in the svn kernel, or I misconfigured something?

 

When I try to build I get this error:

 

`.devexit.text' referenced in section `.data' of drivers/built-in.o: defined in discarded section `.devexit.text' of drivers/built-in.o

make: *** [.tmp_vmlinux1] Error 1

 

 

Disabling that and using bfin_nand compiled ok.(which is deprecated)

 

I think with 2.6.24 this worked for me.

 

Toolchain is svn. CPU is BF532-0.5.

 

Thanks.

 

Regards,

 

Andras

QuoteReplyEditDelete

 

 

2008-11-10 09:55:35     Re: trunk platform nand driver

Mike Frysinger (UNITED STATES)

Message: 64941   

 

the nand platform driver builds fine for me with the BF537-STAMP config

 

run make with CONFIG_DEBUG_SECTION_MISMATCH=y to try and get a better idea of where this reference is coming from ... the built-in.o objects are a bunch of drivers combined

QuoteReplyEditDelete

 

 

2008-11-10 13:46:36     Re: trunk platform nand driver

Andras Szemzo (HUNGARY)

Message: 64967   

 

it does't sad to much new info for me, but repulling a fresh and clean svn and adding my custom board files solved the problem...

 

Thanks for the help and the info

 

Regards,

 

Andras

Attachments

    Outcomes