2008-11-06 02:12:11     DHCP server

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-11-06 02:12:11     DHCP server

vijai ragavan (INDIA)

Message: 64730   

 

Hai,

 

How to enable the DHCP server on uClinux?

QuoteReplyEditDelete

 

 

2008-11-06 02:44:45     Re: DHCP server

Mike Frysinger (UNITED STATES)

Message: 64731   

 

it's like any other package.  select it in the vendor/user menuconfig system.

QuoteReplyEditDelete

 

 

2008-11-06 04:06:51     Re: DHCP server

vijai ragavan (INDIA)

Message: 64737   

 

hai,

 

it is defaultly selected in the 2008R1 distribution .

 

user setting-->Network Application---> [*] dhcpcd-new (2.0/2.4)   .

 

This is my teraterm output.

 

root:/> ifconfig

eth0      Link encap:Ethernet  HWaddr 00:11:22:33:00:00

          inet addr:172.16.6.216  Bcast:172.16.255.255  Mask:255.255.0.0

          UP BROADCAST NOTRAILERS RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:2552 errors:0 dropped:0 overruns:0 frame:0

          TX packets:10 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

                    Interrupt:82 Base address:0x600 DMA chan:ff

 

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          UP LOOPBACK RUNNING  MTU:16436  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

 

root:/>

 

 

 

 

QuoteReplyEditDelete

 

 

2008-11-06 04:37:01     Re: DHCP server

Mike Frysinger (UNITED STATES)

Message: 64764   

 

did you  have a question ?

QuoteReplyEditDelete

 

 

2008-11-06 06:11:46     Re: DHCP server

vijai ragavan (INDIA)

Message: 64765   

 

hai,

 

that DHCP server is enabled in the user setting.Eventhough ftpget is not working.

 

tetaterm output:

 

root:/> ftpget -u raghavan -p raghavan 172.16.6.180 /bin/VOD VOD

ftpget: cannot connect to remote host (172.16.6.180): Network is unreachable

root:/>

 

 

 

Why it shows cannot connect to remote host (172.16.6.180): Network is unreachable?Is it necessory to modify anything?

QuoteReplyEditDelete

 

 

2008-11-06 06:16:59     Re: DHCP server

Mike Frysinger (UNITED STATES)

Message: 64766   

 

it would appear your network is not properly configured (either the physical ethernet cables/switches or software)

 

please read:

http://docs.blackfin.uclinux.org/doku.php?id=setting_up_the_network

QuoteReplyEditDelete

 

 

2008-11-06 14:20:59     Re: DHCP server

Robin Getz (UNITED STATES)

Message: 64780   

 

Vijai:

 

You keep talking about "DHCP server" - but you are pointing to the DHCP Client.

 

What exactly are you looking for?

 

Both are covered on the wiki - just search.

 

-Robin

Attachments

    Outcomes