2008-10-30 08:41:49     BF537 Sport Driver

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-30 08:41:49     BF537 Sport Driver

Daniele Pagani (ITALY)

Message: 64439   

 

Hi,

 

I'm reading this one from an old post (2006-04-05)

 

"As for what other people have been asking for - is a user space access to sport (/dev/sport0 , /dev/sport1), where they could have some sort of setup structure (to configure things), and then ioctl for dma_setup (read_buf, write_buf, num_samples); and a dma_go. Some people have asked for double buffers, so that they don't have to worry about loosing data.

 

The desire is for non-blocking functions (call the function, like dma_start(), and it starts, and then signals the app via the poll() interface when it is done, or a buffer is full)."

 

Is there some news about the matter?

 

Somebody has develop a double buffers?

 

Best regards,

 

Daniele.

TranslateQuoteReplyEditDelete

 

 

2008-10-30 14:19:08     Re: BF537 Sport Driver

Mike Frysinger (UNITED STATES)

Message: 64457   

 

the char sport driver has not been extended in a very long time.  the only ioctl that exists atm is for configuring things.

Attachments

    Outcomes