2008-10-23 02:32:20     BSPs for video door bell (VLC based)

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-23 02:32:20     BSPs for video door bell (VLC based)

xabi romero (UNITED STATES)

Message: 64087   

 

Could anybody tell me how it works?

is like the current video door bell sistem? (first you call to the user and

then when the user takes the phone, the comunication starts: Tx the video from

the street to the house with the audio and  so on..)

is a bidirectional audio transmision?

how long is the video latency?

Thanks and regards

 

QuoteReplyEditDelete

 

 

2008-10-23 03:28:58     Re: BSPs for video door bell (VLC based)

Mike Frysinger (UNITED STATES)

Message: 64092   

 

the demo just uses linphone in video mode.  there is no smarts in terms of an actual "video doorbell system" prototype.  we call the linphone in video mode a "video doorbell system" because that is what it demonstrates in terms of capabilities -- live two way video and audio.  all the rest is up to the end customer to implement.

QuoteReplyEditDelete

 

 

2008-10-23 03:37:52     Re: BSPs for video door bell (VLC based)

xabi romero (UNITED STATES)

Message: 64093   

 

OK Myke

 

Thank you very much

 

regards

QuoteReplyEditDelete

 

 

2008-10-27 05:27:10     Re: BSPs for video door bell (VLC based)

Sonic Zhang (CHINA)

Message: 64224   

 

Actaull, the video door bell demo is based on VLC not linphone.

 

 

 

Sonic

QuoteReplyEditDelete

 

 

2008-10-27 05:39:21     Re: BSPs for video door bell (VLC based)

Yi Li (CHINA)

Message: 64225   

 

VLC is only used for video streaming. Linphone demos the video door bell application using two way audio and one way video.

Attachments

    Outcomes