2008-10-23 03:20:31     Kernel Compilation Error

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-23 03:20:31     Kernel Compilation Error

Ammar Asi (PAKISTAN)

Message: 64090   

 

Hi,

 

I am trying to build the kernal (uClinux-dist-2007R1-RC3) for the IP04 PBX board (BF532). Here is the procedure I am following

 

$ make menuconfig

 

Default options, just selected the Target architecture

 

$ make

 

It asks for the 'general options', I almost selected the default ones.

 

But make gives error:

 

  CC      init/version.o

  LD      init/built-in.o

  LD      .tmp_vmlinux1

kernel/built-in.o:(.data+0xd28): undefined reference to `sysctl_pagecache_ratio_sysctl_handler'

make[2]: *** [.tmp_vmlinux1] Error 1

make[2]: Leaving directory `/root/Documents/astfin/build_ip04/uClinux-dist/linux-2.6.x'

make[1]: *** [linux] Error 1

make[1]: Leaving directory `/root/Documents/astfin/build_ip04/uClinux-dist'

make: *** [uClinux] Error 2

 

Please help......

 

QuoteReplyEditDelete

 

 

2008-10-23 03:24:36     Re: Kernel Compilation Error

Mike Frysinger (UNITED STATES)

Message: 64091   

 

none of the uclinux-dist's supported the IP04 board.  you'll need to get the dist from the IP04 guys and then ask them build error questions.

 

you should start here:

http://blackfin.uclinux.org/gf/project/asterisk/

Attachments

    Outcomes