2008-10-23 02:58:05     Ad1836 driver

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-23 02:58:05     Ad1836 driver

Daniele Pagani (ITALY)

Message: 64089   

 

Hi guys,

 

I'm using ad1836 driver with Ezkit BF537 and audio works fine.

 

(I don't need to change anything to run audio on Ezkit instead Stamp board with this driver).

 

I'm using:

 

vrec -w -s 48000 -b 16 | vplay

 

in order to put on audio output what I receive on audio input.

 

But, 2 questions:

 

1) is it possible using audio at 24bit and not only at 16 bit? Is it depent by vplay/vrec or it is a problem in the driver implementation?

 

2) I'm seeing a delay of about 25ms that is 1024 sample at 48Khz; where can I reduce this delay (I suppose that it is a size of a buffer in the driver implementation)

 

Many thanks,

 

Daniele.

Attachments

    Outcomes