2008-10-16 17:17:34     SPI_MMC and AD1836

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-16 17:17:34     SPI_MMC and AD1836

Guillaume Duteil (FRANCE)

Message: 63811   

 

Good evening,

 

I am working on a sound gateway based on BF533, AD1836 and MMC/SD card on SPI.

 

I am facing a problem using MMC and AD1836 in the same time. When I mount the MMC, the AD1836 driver doesn't load, and if I load the AD1836 before mounting the MMC, I can't mount the partition.

 

Is there a way to make both work in the same time ?

 

Are there other "easy" ways to access MMC cards and free the SPI bus for the AD1836 ?

 

 

 

Thank you un advance

 

 

 

Guillaume Duteil

 

 

TranslateQuoteReplyEditDelete

 

 

2008-10-16 22:24:59     Re: SPI_MMC and AD1836

Yi Li (CHINA)

Message: 63815   

 

Hi,

 

There may be two aspects for your issue:

 

1. Does you spi_mmc use the same SPI_CS pin as the AD1836?

 

2. Currently, spi_mmc cannot share SPI bus with other SPI devices (otherwise spi_mmc cannot work properly). We are still working to solve this issue from software side. (Some people suggest emulate SPI using SPORT but we don't support this currently. Also you may think of using GPIO to emulate SPI (please refer to linux/drivers/spi/spi_bitbang.c), for AD1836, I think this could work).

 

-Yi

QuoteReplyEditDelete

 

 

2008-10-17 00:29:37     Re: SPI_MMC and AD1836

Mike Frysinger (UNITED STATES)

Message: 63823   

 

post the actual errors you're seeing instead of vague high level terms

QuoteReplyEditDelete

 

 

2008-10-17 04:26:58     Re: SPI_MMC and AD1836

Guillaume Duteil (FRANCE)

Message: 63847   

 

Thank you I will look at spi_bitbang

TranslateQuoteReplyEditDelete

 

 

2008-10-22 10:18:24     Re: SPI_MMC and AD1836

Steve Strobel (UNITED STATES)

Message: 64046   

 

I have spi_bitbang working on the AD1938, for which I adapted the AD1836 driver (they are somewhat similar).  I think you can find the SPI driver in the file https://blackfin.uclinux.org/gf/download/forummessage/60926/5184/ad1938codecdriverandnotes.zip.

 

Steve

Attachments

    Outcomes