2008-10-21 10:44:20     Problems with BlueTechnix CM-BF537E

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-21 10:44:20     Problems with BlueTechnix CM-BF537E

Patrick Hotz (GERMANY)

Message: 63992   

 

Please Help me,

 

i have big problems with my CM-BF537E on a FireCracker Board...

at the moment there is the BlueSheep bootloader installed

 

 

 

I connect to the board using the minicom terminal software under Debian.

 

I have connection to the board.

but i can not send the u-boot .hex file to the CM-BF537E...

 

 

 

i have read the FAQ from BlueTechnix but it doesent work..

(http://bluetechnix.at/rainbow2006/site/support/faq/350/faq.aspx)

 

 

 

i start the transfer with "xmr u-boot.hex" ==> that is OK

then i start the file transfer using xmodem config ==> the CM-BF537E Module hangs up and do nothing until i press the reset button...

 

 

 

is there anyone who can help me?

 

 

 

TranslateQuoteReplyEditDelete

 

 

2008-10-21 13:51:52     Re: Problems with BlueTechnix CM-BF537E

Mike Frysinger (UNITED STATES)

Message: 63997   

 

we dont use/know/support the Blue/Black Sheep bootloaders.  you'll have to contact the BlueTechnix guys for assistance.

 

QuoteReplyEditDelete

 

 

2008-10-21 15:45:36     Re: Problems with BlueTechnix CM-BF537E

Robin Getz (UNITED STATES)

Message: 64001   

 

Patrick:

 

We don't support the Firecracker board either. As Mike said - ask your place of purchase for support.

 

-Robin

Attachments

    Outcomes