2008-10-20 04:47:32     Windows-Computer <> BF537, network connection problem

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-20 04:47:32     Windows-Computer <> BF537, network connection problem

Edwin Oyaga (GERMANY)

Message: 63933   

 

 

 

Good day everybody,

 

I am having some troubles trying to build a network connection between a windows-Computer and the BF537 (uClinux). Right now I am using a work around: the BF537 pings the host computer right after booting. After this, the host-computer is able to see (to ping) the BF537. 

 

Does anyone know, what needs to be changed in the uClinux-Config in order to see the bf537 without bf537 pinging any Host-Computer?

 

Thanks for the suggestions.

 

- Edwin

QuoteReplyEditDelete

 

 

2008-10-20 05:38:52     Re: Windows-Computer <> BF537, network connection problem

Mike Frysinger (UNITED STATES)

Message: 63939   

 

what version of software are you using (u-boot/toolchain/uclinux-dist) ?  *when* do you do the ping (in u-boot/Linux/etc....) ?

 

post the full booting output as well as `ifconfig` on the interface

QuoteReplyEditDelete

 

 

2008-10-21 12:21:16     Re: Windows-Computer <> BF537, network connection problem

Edwin Oyaga (GERMANY)

Message: 63994   

 

Hello Mike,

 

the versions are:

 

uClinux-Version: 2006R2

Tool Chain: Toolchain Release 2006R2

u-boot: uboot_1.1.3 Release 2006R2

 

I actually do the ping when uClinux is running (rc - file)

 

please check the files for more info.

 

Thanks in advance.

 

- Edwin

 

ifconfig_output.txt

bootphase_output.txt

QuoteReplyEditDelete

 

 

2008-10-21 13:50:53     Re: Windows-Computer <> BF537, network connection problem

Mike Frysinger (UNITED STATES)

Message: 63995   

 

that's an awfully old release ... do you only have the network problems with that one windows machine, or is it any external machine ?

 

use wireshark and see if the Blackfin board responds to any machines

Outcomes