2008-10-17 08:06:19     2007R1 svn branch

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-17 08:06:19     2007R1 svn branch

Tinku Jose (INDIA)

Message: 63849   

 

Hi,

 

while trying to download 2007R1 svn branch

 

(svn://blackfin.uclinux.org/linux-kernel/branches/2007R1)

 

*******************************************************

 

A    2007R1/include/linux/netfilter_ipv4

A    2007R1/include/linux/netfilter_ipv4/ipt_limit.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_proto_gre.h

A    2007R1/include/linux/netfilter_ipv4/ipt_helper.h

A    2007R1/include/linux/netfilter_ipv4/ip_nat_protocol.h

A    2007R1/include/linux/netfilter_ipv4/ipt_recent.h

A    2007R1/include/linux/netfilter_ipv4/ipt_state.h

A    2007R1/include/linux/netfilter_ipv4/ipt_SAME.h

A    2007R1/include/linux/netfilter_ipv4/ipt_ah.h

A    2007R1/include/linux/netfilter_ipv4/ipt_owner.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_irc.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_h323.h

A    2007R1/include/linux/netfilter_ipv4/ip_nat_helper.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack.h

A    2007R1/include/linux/netfilter_ipv4/ipt_policy.h

A    2007R1/include/linux/netfilter_ipv4/ipt_comment.h

A    2007R1/include/linux/netfilter_ipv4/ipt_tos.h

A    2007R1/include/linux/netfilter_ipv4/ipt_ULOG.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_core.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_ftp.h

A    2007R1/include/linux/netfilter_ipv4/ipt_dccp.h

A    2007R1/include/linux/netfilter_ipv4/ipt_tcpmss.h

A    2007R1/include/linux/netfilter_ipv4/ipt_addrtype.h

A    2007R1/include/linux/netfilter_ipv4/ipt_CLASSIFY.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_protocol.h

A    2007R1/include/linux/netfilter_ipv4/ipt_LOG.h

A    2007R1/include/linux/netfilter_ipv4/ipt_conntrack.h

A    2007R1/include/linux/netfilter_ipv4/ip_nat_rule.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_sctp.h

A    2007R1/include/linux/netfilter_ipv4/ipt_dscp.h

A    2007R1/include/linux/netfilter_ipv4/ipt_DSCP.h

A    2007R1/include/linux/netfilter_ipv4/ipt_mark.h

A    2007R1/include/linux/netfilter_ipv4/ipt_MARK.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_helper.h

A    2007R1/include/linux/netfilter_ipv4/ipt_multiport.h

A    2007R1/include/linux/netfilter_ipv4/ipt_mac.h

A    2007R1/include/linux/netfilter_ipv4/ip_nat_pptp.h

A    2007R1/include/linux/netfilter_ipv4/ipt_ttl.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_tcp.h

A    2007R1/include/linux/netfilter_ipv4/ipt_ecn.h

A    2007R1/include/linux/netfilter_ipv4/ipt_TOS.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_icmp.h

A    2007R1/include/linux/netfilter_ipv4/ipt_NFQUEUE.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_helper_h323_types.h

A    2007R1/include/linux/netfilter_ipv4/ipt_hashlimit.h

A    2007R1/include/linux/netfilter_ipv4/ipt_iprange.h

A    2007R1/include/linux/netfilter_ipv4/ipt_esp.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_tftp.h

A    2007R1/include/linux/netfilter_ipv4/ipt_realm.h

A    2007R1/include/linux/netfilter_ipv4/ipt_pkttype.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_pptp.h

A    2007R1/include/linux/netfilter_ipv4/ipt_TTL.h

A    2007R1/include/linux/netfilter_ipv4/ipt_connbytes.h

A    2007R1/include/linux/netfilter_ipv4/ipt_ECN.h

A    2007R1/include/linux/netfilter_ipv4/ipt_string.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_tuple.h

A    2007R1/include/linux/netfilter_ipv4/Kbuild

A    2007R1/include/linux/netfilter_ipv4/ipt_TCPMSS.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_helper_h323_asn1.h

A    2007R1/include/linux/netfilter_ipv4/ipt_length.h

A    2007R1/include/linux/netfilter_ipv4/ipt_physdev.h

A    2007R1/include/linux/netfilter_ipv4/ip_tables.h

A    2007R1/include/linux/netfilter_ipv4/ip_nat.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_amanda.h

A    2007R1/include/linux/netfilter_ipv4/ip_queue.h

A    2007R1/include/linux/netfilter_ipv4/ip_nat_core.h

A    2007R1/include/linux/netfilter_ipv4/ipt_connmark.h

A    2007R1/include/linux/netfilter_ipv4/ipt_CONNMARK.h

A    2007R1/include/linux/netfilter_ipv4/ip_conntrack_sip.h

A    2007R1/include/linux/netfilter_ipv4/ipt_sctp.h

A    2007R1/include/linux/netfilter_ipv4/ipt_CLUSTERIP.h

A    2007R1/include/linux/netfilter_ipv4/ipt_REJECT.h

svn: In directory '2007R1/include/linux/netfilter_ipv4'

svn: Can't move source to dest

svn: Can't move '2007R1/include/linux/netfilter_ipv4/.svn/tmp/prop-base/ipt_DSCP

.h.svn-base' to '2007R1/include/linux/netfilter_ipv4/.svn/prop-base/ipt_DSCP.h.s

vn-base': No such file or directory

 

 

**********************************************

 

i've tried with different version of tortoise svn client and standart svn client

 

is there any tar.gz for the 2007R1 svn branch available.

 

best regards

 

tinku

 

 

QuoteReplyEditDelete

 

 

2008-10-17 11:51:38     Re: 2007R1 svn branch

Robin Getz (UNITED STATES)

Message: 63853   

 

Tinku:

 

What is your host? Both the Linux kernel and the uClinux-dist require a POSIX compilant file system.

 

-Robin

QuoteReplyEditDelete

 

 

2008-10-17 11:53:04     Re: 2007R1 svn branch

Mike Frysinger (UNITED STATES)

Message: 63854   

 

as Robin indicates, case insensitive filesystems are not supported.  that means no Windows.

QuoteReplyEditDelete

 

 

2008-10-17 12:16:21     Re: 2007R1 svn branch

Tinku Jose (INDIA)

Message: 63857   

 

Hi Robin, Mike,

 

Thanks for the input, infact i was trying earlier with windows/cygwin but later i tried with linux and it started... So currently i am downloading. Thought i will update after both are completed. thanks again

 

best regards

 

tinku

Attachments

    Outcomes