2008-10-15 04:16:39     Cache Table doubts in 2007 R1

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-15 04:16:39     Cache Table doubts in 2007 R1

Appalayagari Sreedhar (INDIA)

Message: 63688   

 

Hi,

 

I am working with custom board with bf533 uClinux distribution 2007 R1. sdram of size 64 MB.

 

I am able to boot the builded uImage, following information comes for Memory Map.

 

## Booting image at 02f00000 ...

   Image Name:   uClinux Kernel and ext2

   Created:      2008-10-12  16:12:19 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    2734472 Bytes =  2.6 MB

   Load Address: 00180000

   Entry Point:  00180000

   Verifying Checksum ... crc32 = 0xe71ed79a

OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 180000

Linux version 2.6.19.3-ADI-2007R1-svn (sreedhar@HDDteam) (gcc version 4.1.1 (ADI

07R1)) #595 Sun Oct 12 21:42:02 IST 2008

 

Blackfin support (C) 2004-2006 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev. 0.5

Blackfin uClinux support by http://blackfin.uclinux.org/

Processor Speed: 594 MHz core clock and 118 Mhz System Clock

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  text      = 0x00180000-0x0029b000

  init      = 0x0029b000-0x002a8ba8

  data      = 0x002ae8e8-0x002e4ce0

  stack     = 0x002b0000-0x002b2000

  bss       = 0x002e4ce0-0x0033207c

  available = 0x0033207c-0x02f00000

  rootfs    = 0x02f00000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

Instruction Cache Enabled

Data Cache Enabled (write-back)

Hardware Trace Enabled

Built 1 zonelists.  Total pages: 11891

 

Kernel command line: root=/dev/mtdblock0 rw,console=ttyBF0,57600

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Physical pages: 2f00

Memory available: 44000k/62789k RAM, (54k init code, 1132k kernel code, 308k dat

a, 1024k dma)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin DATA_A SRAM: 16 KB

Blackfin DATA_B SRAM: 16 KB

Blackfin Instruction SRAM: 64 KB

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 512 (order: -1, 2048 bytes)

TCP established hash table entries: 2048 (order: 1, 8192 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 2048 bind 1024)

TCP reno registered

 

io scheduler noop registered (default)

 

Single Core  Loader Module enabled

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

RAMDISK driver initialized: 1 RAM disks of 4096K size 1024 blocksize

Network interface: "eth0"<6>/proc/HW_ADDR created

ret value from smsc911x_drv_probe Func is 0

uclinux[mtd]: RAM probe address=0x2f00000 size=0x1000000

Creating 1 MTD partitions on "RAM":

0x00000000-0x01000000 : "ROMfs"

uclinux[mtd]: set ROMfs:EXT2  to be root filesystem

rtc-bfin rtc-bfin: rtc intf: sysfs

rtc-bfin rtc-bfin: rtc intf: proc

rtc-bfin rtc-bfin: rtc intf: dev (254:0)

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

 

CP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting the system clock to 1970-01-01 00:00:58 (58)

VFS: Mounted root (ext2 filesystem) readonly.

Freeing unused kernel memory: 52k freed (0x29b000 - 0x2a7000)

dma_alloc_init: dma_page @ 0x00497000 - 256 pages at 0x03f00000

SIOCADDRT: No such device

 

 

BusyBox v1.4.1 (2008-10-12 14:41:30 IST) Built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

#

 

Kernel entry point is 0x180000,

 

When i saw the cache table entries using VDSP window after booting the uImage. i could see that there are 2 entries has the same start address as 0x00000000 in ICPLB_ADDRx and DCPLB_ADDRx. I am attaching the snapshot of the same details. because of this i am getting exception 27.

 

I feel i am doing some mistake. Can you please suggest me what i am doing wrong?. Please let me know if you need further info.

 

Best Regards, Sreedhar.

QuoteReplyEditDelete

 

 

2008-10-15 04:27:25     Re: Cache Table doubts in 2007 R1

Robin Getz (UNITED STATES)

Message: 63710   

 

Sreedhar:

 

Do not connect VDSP - it can cause problems for the kernel.

 

If you want a JTAG emulator - use gdb.

 

The overlapping CPLB tables are expected, and desired. That is the only way to catch null pointers. See /proc/dcplb

 

-Robin

Attachments

    Outcomes