2008-10-08 05:57:19     need image viwer in uclinux for bf537

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-08 05:57:19     need image viwer in uclinux for bf537

suresh kumar (INDIA)

Message: 63259   

 

I need image viewer for uclinux for bf 537.For Graphical view i am using DDD and Gnu plotting was used for plooting application.i need image viewer.How do to this?.

 

 

 

One more issues:

 

i followed this docum link

 

http://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:sdl

Examples

 

SDL has many demos, games, and applications applications which you can look at and examine the source code. A select few of these examples are included in the uClinux-dist. You can build these by selecting Blackfin app programs → [ ] SDL Examples.

 

 

 

but i am not getting SDL option in Blackfin app programs → [ ] SDL

 

 

 

there is no such a option.

 

─────────────────────────────────────── Blackfin app programs ────────────────────────────────────────────────────────────────┐

  │  Arrow keys navigate the menu.  <Enter> selects submenus --->.  Highlighted letters are hotkeys.  Pressing <Y> includes, <N> excludes, <M>           │

  │  modularizes features.  Press <Esc><Esc> to exit, <?> for Help.  Legend: [*] built-in  [ ] excluded  <M> module  < > module capable                  │

  │                                                                                                                                                      │

  │                                                                                                                                                      │

  │ ┌──────────────────────────────────────────────────────────────────────────────────────────────────────────────────────────────────────────────────┐ │

  │ │                                                      [*] Sqlite, a light weight database                                                         │ │

  │ │                                                      [ ] lmbench                                                                                 │ │

  │ │                                                      [*] strace                                                                                  │ │

  │ │                                                      [ ] devtest                                                                                 │ │

  │ │                                                      [ ] devout                                                                                  │ │

  │ │                                                      [*] rsh                                                                                     │ │

  │ │                                                      [*] rcp                                                                                     │ │

  │ │                                                      [*] rshd                                                                                    │ │

  │ │                                                      [*] oprofile                                                                                │ │

  │ │                                                      [ ] watchdog simple deamon                                                                  │ │

  │ │                                                      [*] yaffs-utils                                                                             │ │

  │ │                                                      [ ] BF561 Core B support tools                                                              │ │

  │ │                                                      [ ] pound SSL Wrapper                                                                       │ │

  │ │                                                      [*] jpegview                                                                                │ │

  │ │                                                      [ ] jpegview DMA Blit/FillRect                                                              │ │

  │ │                                                      [ ] pngview                                                                                 │ │

  │ │                                                      [*] IRDA Tools (irattach)                                                                   │ │

  │ │                                                      [ ] ALSA utils                                                                              │ │

  │ │                                                      [ ] Asterisk PBX                                                                            │ │

  │ │                                                      [ ] usbutils (lsusb)                                                                        │ │

  │ │                                                      [ ] Bluez-utils                                                                             │ │

  │ │                                                      [ ] picocom                                                                                 │ │

  │ │                                                                 

 

 

QuoteReplyEditDelete

 

 

2008-10-08 07:04:48     Re: need image viwer in uclinux for bf537

Robin Getz (UNITED STATES)

Message: 63260   

 

Suresh:

 

The documentation reflects the latest release. You are not using that.

 

Upgrade.

 

-Robin

QuoteReplyEditDelete

 

 

2008-10-08 07:06:42     Re: need image viwer in uclinux for bf537

Robin Getz (UNITED STATES)

Message: 63261   

 

As for your request for an image viewer - you aren't specific if you want the image viewer to run on the Blackfin (there are a few, depending on what types of images you want to look at) or on the host (via a debugger). It appears to be the latter, but I'm not sure.

 

-Robin

QuoteReplyEditDelete

 

 

2008-10-10 01:46:16     Re: need image viwer in uclinux for bf537

suresh kumar (INDIA)

Message: 63366   

 

Dear Robin.

 

I need the image viewer for image processing exprementel.for ploting kind application we can use GNUPloting.Like That Image what kind options are there in uclinux.

QuoteReplyEditDelete

 

 

2008-10-10 10:39:06     Re: need image viwer in uclinux for bf537

Robin Getz (UNITED STATES)

Message: 63422   

 

Suresh:

 

I still have no idea what you are asking for. (sorry).

 

What are you trying to do?

QuoteReplyEditDelete

 

 

2008-10-13 06:12:06     Re: need image viwer in uclinux for bf537

suresh kumar (INDIA)

Message: 63541   

 

Dear Robin,

 

If we want to see any jpg image.how can see the image in bf537 under uclinux.

 

suresh

 

 

QuoteReplyEditDelete

 

 

2008-10-13 06:28:20     Re: need image viwer in uclinux for bf537

Yi Li (CHINA)

Message: 63546   

 

Firstly  you need a video display device (e.g LCD), and a device driver for this device. For application, you can use jpegview (which decode jpeg and output the display device).

Attachments

    Outcomes