2008-10-10 02:20:43     No BF537-EZKIT available in make menuconfig...

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-10 02:20:43     No BF537-EZKIT available in make menuconfig...

Jere Mäkelä (FINLAND)

Message: 63368   

 

I have two eval. boards: BF533 Stamp and BF537 EZ-kit. I updated uclinux to 533 board ok but now as I try to do the same with 537, I cannot get an option to select BF537-EZ-kit.

 

procedures:

 

root> make clean

 

root> make menuconfig

 

-> Select the Vendor...Only gives Analog Devices

 

-> Select the Product...Only gives BF533-STAMP

 

 

 

????

 

Jere

QuoteReplyEditDelete

 

 

2008-10-10 02:34:00     Re: No BF537-EZKIT available in make menuconfig...

Daniele Pagani (ITALY)

Message: 63369   

 

Dear Jere,

 

I've the BF537-Ezkit too, and I can select the "BF537-STAMP" voice under "AnalogDevices Products".

 

I've the uClinux-dist-2008R1.5-RC3, so I think that you've not this release.

 

Please, update yours to this one.

 

Best regards,

 

Daniele.

TranslateQuoteReplyEditDelete

 

 

2008-10-10 03:09:46     Re: No BF537-EZKIT available in make menuconfig...

Yi Li (CHINA)

Message: 63373   

 

You can build kernel for BF537-STAMP and run on BF537-ezkit. For difference of the two, please refer to: http://docs.blackfin.uclinux.org/doku.php?id=hw:boards:bf537-ezkit

Attachments

    Outcomes