2008-10-09 09:52:25     Partial success with serial-console output.

Document created by Aaronwu Employee on Aug 8, 2013
Version 1Show Document
  • View in full screen mode

2008-10-09 09:52:25     Partial success with serial-console output.

Thomas Langås (NORWAY)

Message: 63335   

 

Ok, so now I've reached to point where I get output from the console after the serial-driver is loaded, but I don't get anything from earlier, even though my bootargs contains the earlyprintk-stuff. The weird thing is that if I do the post-mortem search, only the console=-part of my commandline shows up, none of the root= or earlyprintk-stuff does.

 

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 2) at 24000300 IRQ 83 [nowait]

eth0: Invalid ethernet MAC address.  Please set using ifconfig

Linux video capture interface: v2.00

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

802.1Q VLAN Support v1.8 Ben Greear <greearb@candelatech.com>

All bugs added by David S. Miller <davem@redhat.com>

Freeing unused kernel memory: 3472k freed

dma_alloc_init: dma_page @ 0x00d91000 - 1024 pages at 0x07c00000

 

What is supposed to be output after this? Only the root-prompt? Where should I begin to look if I don't get this?

QuoteReplyEditDelete

 

 

2008-10-09 12:29:01     Re: Partial success with serial-console output.

Mike Frysinger (UNITED STATES)

Message: 63341   

 

everything after dma_alloc_init is userspace.  make sure you have a shell actually launch on the console via init.

Attachments

    Outcomes