2008-08-08 06:43:26     2008R1 uImage Issue

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-08-08 06:43:26     2008R1 uImage Issue

kang p (INDIA)

Message: 60159   

 

Hi ,

 

I'm facing issue in booting of my target platform bf533 - custom hardware.

 

Using 2008 R1 distribution.Please find the log below.

 

## Booting image at 01200000 ...

   Image Name:   Linux-2.6.22.18-ADI-2008R1-svn

   Created:      2008-08-08  10:55:14 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4085253 Bytes =  3.9 MB

   Load Address: 00300000

   Entry Point:  0044c000

addr = 1200000

len = 3e5605

data = 1200040

   Verifying Checksum ... crc32 = fed323e1

OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 44c000

 

 

 

It was working fine ,after i enabled few options in the kernel hacking (make menuconfig) this problem occurs.

 

I couldnt revert back.What could be the reason for this uImage bootup hang?

 

Thanks

QuoteReplyEditDelete

 

 

2008-08-08 09:48:19     Re: 2008R1 uImage Issue

Robin Getz (UNITED STATES)

Message: 60162   

 

Kang:

 

Without knowing why it is crashing - there isn't much help we can give.

 

You can find out why, by following the directions at:

 

http://docs.blackfin.uclinux.org/doku.php?id=post_mortem

 

 

 

-robin

Attachments

    Outcomes