2008-10-05 09:20:16     Serial number in CM-BF537

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-10-05 09:20:16     Serial number in CM-BF537

Miquel Soler i Mir (SPAIN)

Message: 63118   

 

Hello.

 

I'm working with CM-BF537 core and I trying to find some serial number in the internal memory.

 

I check with the datasheet and I can't found.

 

The idea is use this to have a serial number.

 

Can somebody help me?

 

Has somebody a better idea?

 

Thanks

 

Miquel Soler i Mir

 

 

 

 

TranslateQuoteReplyEditDelete

 

 

2008-10-05 14:58:15     Re: Serial number in CM-BF537

Mike Frysinger (UNITED STATES)

Message: 63121   

 

you should contact the Bluetechnix guys seeing as how they're the ones who made it

 

http://www.bluetechnix.com/rainbow2006/Default.aspx

QuoteReplyEditDelete

 

 

2008-10-05 16:37:43     Re: Serial number in CM-BF537

Hubert Kleis (SPAIN)

Message: 63126   

 

Mike,

 

you've got Miquel wrong.

 

The question was about a serial number of the BF357(E), not the Bluetechnix board.

 

Is there a way to get the serial of the chip?

 

Best regards

 

Hubert

QuoteReplyEditDelete

 

 

2008-10-05 16:49:25     Re: Serial number in CM-BF537

Mike Frysinger (UNITED STATES)

Message: 63127   

 

there is no such thing a serial number with the BF53x processors.  there are only part numbers.

QuoteReplyEditDelete

 

 

2008-10-05 16:52:49     Re: Serial number in CM-BF537

Hubert Kleis (SPAIN)

Message: 63128   

 

well, that's why we didn't find anything digging into the hardware manuals...

 

thanks

 

hubert

Attachments

    Outcomes