2008-09-30 15:15:01     buildind uclinux from trunk

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-09-30 15:15:01     buildind uclinux from trunk

Omar Chanouha (UNITED STATES)

Message: 62949   

 

My setup: toolchain, uclibc, dist = r1.5 on fedora 9. I make menuconfig and selected BF548-ezkit and then answered 'default' to all the config questions. I then typed make and got the following errors:

 

util.o: In function `init_resource_track':

 

../../e2fsprogs-1.40.9/e2fsck/util.c:285: undefined reference to `_sbrk'

 

util.o: In function `print_resource_track':

 

../../e2fsprogs-1.40.9/e2fsck/util.c:336: undefined reference to `_sbrk'

 

collect2: ld returned 1 exit status

 

make[5]: *** [e2fsck] Error 1

 

make[5]: Leaving directory `/home/icteam/Desktop/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.40.9/e2fsck'

 

make[4]: *** [install-progs-recursive] Error 1

 

make[4]: Leaving directory `/home/icteam/Desktop/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.40.9'

 

make[3]: *** [all] Error 2

 

make[3]: Leaving directory `/home/icteam/Desktop/uclinux-dist/user/e2fsprogs'

 

make[2]: *** [e2fsprogs] Error 2

 

What am I doing wrong? Is there a .config somewhere I can use? I have succesfully compiled the release distro with this setup.

 

Thanks!

QuoteReplyEditDelete

 

 

2008-09-30 15:29:53     Re: buildind uclinux from trunk

Mike Frysinger (UNITED STATES)

Message: 62950   

 

please read the FAQ:

http://docs.blackfin.uclinux.org/doku.php?id=faq

 

(Why do I need to use the same version of toolchain/kernel/uClibc/U-boot/uClinux-dist?)

QuoteReplyEditDelete

 

 

2008-09-30 15:45:15     Re: buildind uclinux from trunk

Omar Chanouha (UNITED STATES)

Message: 62952   

 

So are does that mean that in order to compile the svn snpashot of uclinux-dist I have to compile the toolchain/uclibc from thier respective svn snapshots?

QuoteReplyEditDelete

 

 

2008-09-30 15:59:58     Re: buildind uclinux from trunk

Mike Frysinger (UNITED STATES)

Message: 62953   

 

that is what the FAQ says ...

 

svn snaps are not tied together ... only the tip

Attachments

    Outcomes