2008-09-30 06:15:45     Problem in booting Compressed image from spi flash

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-09-30 06:15:45     Problem in booting Compressed image from spi flash

Prathika R (INDIA)

Message: 62923   

 

hi all,

 

we have been trying to boot the compressed image of uClinux from spi flash.

 

I had been successful in writing the compressed image into 4th sector of spi flash using eeprom write command.

 

For booting from spi flash i did something like this in my customised .h file for my board in u-boot.

 

1)i enabled CONFIG_SPI.

 

2)I changed CONFIG_BOOTCMD to "eeprom read 0x1000000 0x40000 0x20c789;bootm 0x20c789".

 

 

 

when i load this .ldr to my board and boot,  it hangs at some point saying Kernel paniced. When i execute commands in uboot command promt like "eeprom read 0x1000000 0x40000 0x20c789" and "md.b 0x1000000  0x1000" to verify the data written to flash, there is no problem in data that is written to flash. Also i tried "tftpboot 0x1000000 uImage" and "bootm 0x1000000" to verify the compressed image. There is no problem in booting, but when it is from flash read, it doesnt boot.

 

I have pasted the entire thing that happens when it tries to boot compressed image from flash.Someone please help me in getting rid of this issue.

 

 

 

Regards,

 

Prathika.R

 

*****************************************************************************************************************

 

U-Boot-1.1.3-ADI-2006R1 (Sep 30 2008 - 09:43:39)

 

CPU:   ADSP BF537 Rev.: 0.2

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 100 MHz

SDRAM: 32 MB

FLASH:   4 MB

Using default environment

 

In:    serial

Out:   serial

Err:   serial

Net:    ADI BF537 EMAC

Hit any key to stop autoboot:  5     0

536bfindas> eeprom read 0x1000000 0x40000 0x20c789

 

EEPROM @0x0 read: addr 01000000  off 40000  count 2148233 ... ################################################################done

536bfindas> bootm 0x1000000

## Booting image at 01000000 ...

   Image Name:   uClinux Kernel and Filesystem

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    2148169 Bytes =  2 MB

   Load Address: 00001000

   Entry Point:  00001000

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... Peeyush:calling inflateInit2

Peeyush:calling inflate

Peeyush:just before inflageEnd

OK

Starting Kernel at = 1000

Linux version 2.6.19.3-ADI-2007R1.12007R1-svn (root@localhost.localdomain) (gcc version 4.1.1 (ADI 07R1)) #29 Wed Sep 24 10:43:49 IST 2008

Warning: limiting memory to 27MB due to hardware anomaly 05000263

Blackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF536 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 225 MHz core clock and 75 Mhz System Clock

Board Memory: 32MB

Kernel Managed Memory: 32MB

Memory map:

  text      = 0x00001000-0x00116498

  init      = 0x00117000-0x00126f2c

  data      = 0x00129194-0x00161aa8

  stack     = 0x0012a000-0x0012c000

  bss       = 0x00161ab0-0x00170b64

  available = 0x00170b64-0x01b00000

  rootfs    = 0x01b00000-0x01f00000

  DMA Zone  = 0x01f00000-0x02000000

Instruction Cache Enabled

Data Cache Enabled (write-back)

Hardware Trace Enabled

Built 1 zonelists.  Total pages: 6845

Kernel command line: root=/dev/mtdblock0 rw console=ttyBF0,115200

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 128 (order: 7, 512 bytes)

Console: colour dummy device 80x25

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Physical pages: 1b00

Memory available: 25808k/31579k RAM, (63k init code, 1109k kernel code, 60k data, 1024k dma)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin DATA_B SRAM: 16 KB

Blackfin Instruction SRAM: 48 KB

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 256 (order: -2, 1024 bytes)

TCP established hash table entries: 1024 (order: 0, 4096 bytes)

TCP bind hash table entries: 512 (order: -1, 2048 bytes)

TCP: Hash tables configured (established 1024 bind 512)

TCP reno registered

io scheduler noop registered

io scheduler anticipatory registered

io scheduler deadline registered

io scheduler cfq registered (default)

pfx: pfbits driver for bf5xx

timer_initialize: module loaded

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

loop: loaded (max 8 devices)

 

Exception: IRQ 0x5 entered

code=[0x0000c026],   stack frame=0x001e7ddc,   bad PC=0x000084c2

----------- HARDWARE ERROR -----------

External Memory Addressing Error

 

CURRENT PROCESS:

 

COMM=swapper PID=1

return address: 0x000084c2; contents of [PC-16...PC+8]:

6c22 e100 5555 9310 0030 0000 0000 0024

0040 0010 0000 3208 e14a 203f e10a 0000 X

9110 6c22 9308 9110 b488 0010 0000 e121

 

RETE:  00000000  RETN: 001e7eb8  RETX: 000084c2  RETS: 000a0f96

IPEND: 8020  SYSCFG: 0036

SEQSTAT: 0000c026    SP: 001e7ddc

R0: 01a448d4    R1: 12345678    R2: 00000006    R3: ffffffff

R4: 0012e910    R5: 000000d4    R6: ffffffc0    R7: 0000003f

P0: 01a448fa    P1: 01a448d4    P2: 203f0000    P3: 01a44800

P4: 01a448d4    P5: 0012e83c    FP: 0012e834

A0.w: 00000000    A0.x: 00000000    A1.w: 00000000    A1.x: 00000000

LB0: ffa01fec  LT0: ffa01fec  LC0: 00000000

LB1: 00080b92  LT1: 00080b88  LC1: 00000000

B0: 0000001a  L0: 00000000  M0: 0012ce00  I0: 001dbe28

B1: 000f4b20  L1: 00000000  M1: 00000000  I1: 001073a4

B2: 00000000  L2: 00000000  M2: 00000000  I2: fffb6c79

B3: 0000ffff  L3: 00000000  M3: 00000000  I3: 00000000

 

USP: 00000000   ASTAT: 02003005

DCPLB_FAULT_ADDR=203f0000

ICPLB_FAULT_ADDR=000084c2

 

 

Kernel panic - not syncing: Unhandled IRQ or exceptions!

 

 

 

 

 

 

QuoteReplyEditDelete

 

 

2008-09-30 10:12:06     Re: Problem in booting Compressed image from spi flash

Mike Frysinger (UNITED STATES)

Message: 62931   

 

2006R1 is a very old release.  upgrade to 2008R1.5 and try again.  the SPI flash driver has been completely rewritten.

Attachments

    Outcomes