2008-09-10 07:26:08     bf 561b.ld file in bfin-elf

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-09-10 07:26:08     bf 561b.ld file in bfin-elf

Pranay Upadhyay (INDIA)

Message: 61883   

 

Hello sir,

 

    I am confusing after seeing the memory allocation in ld file...Please clear these things

 

  In the  bf 561b.ld  file you are giving the B_MEM_* are for  Core A memory region . 

 

  Although in the bf 561a.ld file  B_MEM_* are for  Core B  Memory region.

 

  Then what is the memory distribution in the bf 561m.ld file? Please clear these things.

 

 

 

  -Regards

 

   Pranay

QuoteReplyEditDelete

 

 

2008-09-10 13:05:48     Re: bf 561b.ld file in bfin-elf

Mike Frysinger (UNITED STATES)

Message: 61899   

 

read the BF561 HRM.  one core cannot access the L1 regions of the other.

QuoteReplyEditDelete

 

 

2008-09-10 22:42:29     Re: bf 561b.ld file in bfin-elf

Pranay Upadhyay (INDIA)

Message: 61915   

 

Hello sir,

 

   I am not asking that what ever you replied.My question was about the naming convention in the bf 561b.ld file. It is different naming convention as  compare to the bf 561a.ld and bf 561m.ld file.Please reply.

 

 

 

   -Thanks & Regards

 

    Pranay

QuoteReplyEditDelete

 

 

2008-09-10 23:35:19     Re: bf 561b.ld file in bfin-elf

Pranay Upadhyay (INDIA)

Message: 61916   

 

Hello sir,

 

   I am not asking that what ever you replied.My question was about the naming convention in the bf 561b.ld file. It is different naming convention as  compare to the bf 561a.ld and bf 561m.ld file.

 

              I think there should be not effect of naming convention. Is any limitation and naming conventoin for use of the

 

     external memory SDRAM for Core A and Core B. For using single core I am able to write and excess the data from SDRAM but when I am using the Dual core I am not able to read write the video data from the SDRAM, in Standalone application.Please reply.

 

 

 

   -Thanks & Regards

 

    Pranay

QuoteReplyEditDelete

 

 

2008-09-11 03:09:01     Re: bf 561b.ld file in bfin-elf

Mike Frysinger (UNITED STATES)

Message: 61928   

 

the conventions are exactly the same

QuoteReplyEditDelete

 

 

2008-09-30 08:00:50     Re: bf 561b.ld file in bfin-elf

Pranay Upadhyay (INDIA)

Message: 62925   

 

Hello sir,

 

      I am using the gcc compiler for standalone application , and generating the elf file for the BF 561.

 

                        How can we put the whole code or object file in particular memory location withot using the section __ attribute__  usinfg linker script file? Please give me the some documentation  or  example about this.

 

     I am facing the problem that I am  not able to put some declaration in the particular memory location using the section __ attribute__  .Please help.

 

 

 

  -Thanks & Regards

    Pranay

 

 

QuoteReplyEditDelete

 

 

2008-09-30 10:09:37     Re: bf 561b.ld file in bfin-elf

Mike Frysinger (UNITED STATES)

Message: 62930   

 

linker scripts are completely documented here:

http://sourceware.org/binutils/docs-2.18/ld/Scripts.html#Scripts

Attachments

    Outcomes