2008-09-11 00:51:18     uclinux on bf531

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-09-11 00:51:18     uclinux on bf531

liang wang (CHINA)

Message: 61918   

 

Why  ADI  do not provided uclinux on bf531?Can any one provide to me ?? I want to transplant the BF533-uclinux on it . Can somebody tell me how to modify??

TranslateQuoteReplyEditDelete

 

 

2008-09-11 03:00:01     Re: uclinux on bf531

Mike Frysinger (UNITED STATES)

Message: 61924   

 

what are you talking about ?  Linux runs perfectly fine on a BF531.  please read the documentation:

http://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:features

QuoteReplyEditDelete

 

 

2008-09-11 06:30:14     Re: uclinux on bf531

liang wang (CHINA)

Message: 61947   

 

Mike ,Thank you !

 

when i make menuconfig ,I don't see bf531 in the cpu type,just 533 527 and so on.

 

I see In that page which describe :" Although the following specific platforms are used to test the Blackfin/uClinux dist, it should be possible to use the uClinux-dist on any robust Blackfin platform, with some minor changes. "

 

 

 

HOW  to change?Which files  should  I have to change in the bf533 EZkit uclinux dist?

TranslateQuoteReplyEditDelete

 

 

2008-09-11 08:01:11     Re: uclinux on bf531

Robin Getz (UNITED STATES)

Message: 61983   

 

Liang:

 

were are you looking in menuconfig? I see:

 

( ) BF531

( ) BF532

( ) BF533

( ) BF534

( ) BF536

(X) BF537

 

( ) BF542

( ) BF544

( ) BF547

( ) BF548

( ) BF549

( ) BF561

 

531 is in the list.

QuoteReplyEditDelete

 

 

2008-09-11 08:30:02     Re: uclinux on bf531

Mike Frysinger (UNITED STATES)

Message: 61987   

 

please search the wiki when you have questions.  there are documents that tell you how to port the kernel to your specific platform.

Attachments

    Outcomes