2008-09-01 02:33:17     filesystem romfs and menuconfig

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-09-01 02:33:17     filesystem romfs and menuconfig

Daniele Pagani (ITALY)

Message: 61459   

 

Dear guys,

 

I don't understand a question.

 

When I use make menuconfig I select the application that I want use with uClinux, so, for example, I disable quit all the applications.

 

But, after I've sucessfully compiled, I find again all the application in the /bin directory, so I believe that the compiler uses the romfs directory instead the selected menu with menuconfig (or with xconfig).

 

So, if I want to do not use some applications, what I need to to:

 

1) deselect in the menu in menuconfig and then delete the application from the romfs?

 

or something else?

 

Thank you in advanced for you cooperation,

 

best regards,

 

Daniele.

TranslateQuoteReplyEditDelete

 

 

2008-09-01 04:14:19     Re: filesystem romfs and menuconfig

Michele d'Amico (ITALY)

Message: 61463   

 

Hi Daniele,

 

> 1) deselect in the menu in menuconfig and then delete the application from the romfs?

 

Right!

 

The config tool doesn't check if some tools become selected/unselected, it just runs a make (first all rule and then romfs rule) for every selcted tool/application but it doesn't do anything for the unselected entries.

 

Regards

 

 

 

--Michele

QuoteReplyEditDelete

 

 

2008-09-01 05:00:22     Re: filesystem romfs and menuconfig

Daniele Pagani (ITALY)

Message: 61466   

 

Grazie,

 

ciao

Attachments

    Outcomes