2008-08-25 09:36:03     bf537 -stamp ---tftp server add

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-08-25 09:36:03     bf537 -stamp ---tftp server add

煜 铁 (CHINA)

Message: 61019   

 

my  enviroment  is  that hardware  bf537-stamp ,OS is uclinux-dist-2008R1-RC8.tar.bz2.

 

I want to set TFTPserver in the bf537-stamp communicate with the host pc (Fedora linux)

 

when   i  am compiling    the kernel , i selet the Tftp an Tftpd  in the  user application item .

 

then  i  write  tftp and ip  of bf537-starmp ,on  the  console  of the host PC , apprear  the Tftp >

 

in the second line ,but  then  i  input ' put  dir/local file   hostpc-dir/filename 'in this line ',after a while  apprear ''tftp  tramsmit

 

out of time  ''' on the third line .how host pc can  be  succesful communicate with  the  bf537-stamp with Tftp protol ,and 

 

bf537 is the server ??

 

 

TranslateQuoteReplyEditDelete

 

 

2008-08-25 13:03:10     Re: bf537 -stamp ---tftp server add

Mike Frysinger (UNITED STATES)

Message: 61034   

 

why not just use rcp to transfer files ?  it's already enabled by default

 

QuoteReplyEditDelete

 

 

2008-08-26 01:47:14     Re: bf537 -stamp ---tftp server add

煜 铁 (CHINA)

Message: 61054   

 

but rcp server is very  large ,we have  only  4mb space in the flash ,ever we try to use the sabam but it is more big for our apllication

TranslateQuoteReplyEditDelete

 

 

2008-08-26 02:37:26     Re: bf537 -stamp ---tftp server add

Mike Frysinger (UNITED STATES)

Message: 61055   

 

uhh, rcp/rsh binaries are very small ... like 40k - 60k a piece ... if you cant squeeze that much into flash, then you've got bigger problems

QuoteReplyEditDelete

 

 

2008-08-26 06:24:04     Re: bf537 -stamp ---tftp server add

煜 铁 (CHINA)

Message: 61092   

 

At first ,I much thank for your Reply。 when  adding  the tftpd in the kernel , i selecte  the item tftp procotol in the networking item,and i select   Tftpd  in the networking application item .I want  to  know  whether  it  have  some other  item  must be selected  ,but i donot selected.

TranslateQuoteReplyEditDelete

 

 

2008-08-26 09:35:32     Re: bf537 -stamp ---tftp server add

Mike Frysinger (UNITED STATES)

Message: 61100   

 

we have never tested running a tftpd server on the Blackfin board itself

Attachments

    Outcomes