2008-08-19 22:45:34     BF536 Kernel Panic

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-08-19 22:45:34     BF536 Kernel Panic

Harvey Sugar (UNITED STATES)

Message: 60698   

 

When uClinux is built for the BF536 processor it panics.  I've tried this on my own BF536 based board and on the BF537-EZKIT.  The BF536 build should work on the BF537 because the only difference is that the BF536 has less SRAM.  Are there any other configuration changes I need to do to run uClinux on the BF536?

 

The console output for the boot up and panic is attached.

 

 

 

panic.txt

QuoteReplyEditDelete

 

 

2008-08-19 22:54:43     Re: BF536 Kernel Panic

Mike Frysinger (UNITED STATES)

Message: 60700   

 

make sure you disabled L1 support in the MAC driver

Attachments

Outcomes