2008-07-22 06:06:30     Problem mounting jffs2

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-07-22 06:06:30     Problem mounting jffs2

Vincent Puig (SPAIN)

Message: 59223   

 

Hi all,

 

I am trying to pass the filesystem from nfs to jffs2, when I boot, I get this:

 

## Booting image at 20040000 ...

   Image Name:   Linux-2.6.22.18-ADI-2008R1-svn

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    742310 Bytes = 724.9 kB

   Load Address: 00001000

   Entry Point:  00138000

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 138000

Linux version 2.6.22.18-ADI-2008R1-svn (vincent@canutet) (gcc version 4.1.2 (ADI svn)) #48 Tue Jul 22 11:52:32 CEST 2008

Hardware Trace Active and Enabled

Warning: limiting memory to 31MB due to hardware anomaly 05000263

Blackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

Board Memory: 32MB

Kernel Managed Memory: 32MB

Memory map:

  text      = 0x00001000-0x000fbbb0

  rodata    = 0x000fc000-0x0012986c

  data      = 0x0012a000-0x00138000

    stack   = 0x0012a000-0x0012c000

  init      = 0x00138000-0x00149000

  bss       = 0x00149000-0x00155050

  available = 0x00155050-0x01eff000

  DMA Zone  = 0x01f00000-0x02000000

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists.  Total pages: 7874

Kernel command line: root=/dev/mtdblock2 rw rootfstype=jffs2 console=ttyBF0,115200

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 128 (order: 7, 512 bytes)

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Memory available: 30076k/32768k RAM, (68k init code, 1002k kernel code, 290k data, 1024k dma, 308k reserved)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (9 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 48 KB (40 KB free)

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

cm_bf537_init(): registering device resources

Generic PHY: Registered new driver

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 1024 (order: 1, 8192 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 1024 bind 1024)

TCP reno registered

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

pfx: pfbits driver for bf5xx

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 20) is a BFIN-UART

arch/blackfin/mach-bf537/boards/cm_bf537.c:bfin_get_ether_addr: Setting Ethernet MAC to a random one

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac: Version 1.1, Blackfin BF53[67] BF527 on-chip Ethernet MAC driver

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Contoller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

TCP cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 1

NET: Registered protocol family 17

NET: Registered protocol family 15

Freeing unused kernel memory: 68k freed

dma_alloc_init: dma_page @ 0x01c53000 - 256 pages at 0x01f00000

Kernel panic - not syncing: No init found.  Try passing init= option to kernel.

 

 

What am I doing wrong, It worked well with nfs and ramfs.

 

Thanks.

QuoteReplyEditDelete

 

 

2008-07-22 11:09:08     Re: Problem mounting jffs2

Robin Getz (UNITED STATES)

Message: 59233   

 

Vincent:

 

You told it :

 

>root=/dev/mtdblock2 rw rootfstype=jffs2

 

Which is good.

 

And compiled JFFS2 into the kernel:

 

> JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

 

which is also good.

 

but it did not find any maps/partitions. Have a look at:

 

https://docs.blackfin.uclinux.org/doku.php?id=linux-kernel:mtd#partitioning

 

 

 

-Robin

QuoteReplyEditDelete

 

 

2008-07-23 05:00:04     Re: Problem mounting jffs2

Vincent Puig (SPAIN)

Message: 59265   

 

Ok, thanks Robin.

 

I am following that, but I don't find the default physical mapping driver "physmap-flash.0", which one should I modify??

 

I think it must be something about the file " arch/blackfin/mach-bf537/boards/cm_bf537.c " which looks like:

 

static struct mtd_partition bfin_spi_flash_partitions[] = {

    {

        .name = "bootloader",

        .size = 0x00040000,

        .offset = 0,

        .mask_flags = MTD_CAP_ROM

    }, {

        .name = "kernel",

        .size = 0xC0000,

        .offset = 0x40000

    }, {

        .name = "file system",

        .size = 0x300000,

        .offset = 0x00100000,

    }

};

 

What should I do here?

QuoteReplyEditDelete

 

 

2008-07-23 15:16:19     Re: Problem mounting jffs2

Robin Getz (UNITED STATES)

Message: 59289   

 

Vincent:

 

First thing is to make sure that your specific flash driver is working/installed properly.

 

What hardware are you testing on? and what flash does it have that you are trying to mount as JFFS2?

 

-Robin

QuoteReplyEditDelete

 

 

2008-07-24 03:55:02     Re: Problem mounting jffs2

Vincent Puig (SPAIN)

Message: 59305   

 

I am using a EVAL board of Bluetechnix, with a Blackfin CM-BF537E module.

 

4MB of Flash Disk.

 

Maybe this helps:

 

Memory Type                                      Start Address   End Address      Size             Comment

 

FLASH Bank0 (PF4 Flag low)         0x20000000     0x201FFFFF       2MB            4MB Micron Flash, MT28F320J3FS-11

 

FLASH Bank1 (PF4 Flag high)        0x20000000     0x201FFFFF       2MB

 

 

 

Was that what you wanted?, If jffs2 is not posible, which one should I use?. Thank you and sorry, as I've already said, I am beginner.

QuoteReplyEditDelete

 

 

2008-07-24 04:14:44     Re: Problem mounting jffs2

Mike Frysinger (UNITED STATES)

Message: 59306   

 

there is no flash driver in the kernel for the tiny board modules.  if you search the forums you may find one.

QuoteReplyEditDelete

 

 

2008-07-24 05:46:16     Re: Problem mounting jffs2

Vincent Puig (SPAIN)

Message: 59344   

 

Mike, I found nothing, could you send me the link if you know somewhere, please?.

 

If flash file system is not posible, which one would you use?, I need the information to keep although the board resets.

 

Thank you in advance.

Attachments

    Outcomes