2008-07-10 05:24:08     Compilation Error: multiple definition of `get_vco'

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-07-10 05:24:08     Compilation Error: multiple definition of `get_vco'

kevin zhou (CHINA)

Message: 58610   

 

Hi, all:

 

Compiling under BF533,

 

Anyone can help me how can deal with this error message:

 

GEN     .version

  CHK     include/linux/compile.h

  UPD     include/linux/compile.h

  CC      init/version.o

  LD      init/built-in.o

  LD      .tmp_vmlinux1

drivers/built-in.o: In function `get_vco':

(.text+0x9648): multiple definition of `get_vco'

arch/blackfin/kernel/built-in.o:(.text+0x880): first defined here

/opt/bin/bfin-uclinux-ld.real: Warning: size of symbol `_get_vco' changed from 28 in arch/blackfin/kernel/built-in.o to 26 in drivers/built-in.o

make[1]: *** [.tmp_vmlinux1] Error 1

make[1]: Leaving directory `/HHBF561-R3/uClinux-dist/linux-2.6.x'

make: *** [linux] Error

 

What should I do, need modify the source code?

 

Thanks very much!

QuoteReplyEditDelete

 

 

2008-07-10 10:09:18     Re: Compilation Error: multiple definition of `get_vco'

Robin Getz (UNITED STATES)

Message: 58624   

 

Kevin:

 

You found a bug. Someone will fix in a bit. You can follow the progress here:

 

http://blackfin.uclinux.org/gf/project/uclinux-dist/tracker/?action=TrackerItemEdit&tracker_item_id=4231

 

-Robin

QuoteReplyEditDelete

 

 

2008-07-10 22:18:17     Re: Compilation Error: multiple definition of `get_vco'

kevin zhou (CHINA)

Message: 58648   

 

Got it, Thanks very much!

QuoteReplyEditDelete

 

 

2008-07-10 23:14:52     Re: Compilation Error: multiple definition of `get_vco'

kevin zhou (CHINA)

Message: 58652   

 

Another question, how to find the fixed files?

 

Which branch you put it in SVN?

 

Many many thanks!

QuoteReplyEditDelete

 

 

2008-07-11 11:09:12     Re: Compilation Error: multiple definition of `get_vco'

Robin Getz (UNITED STATES)

Message: 58691   

 

Kevin:

 

The best way is to goto the bug link I posted in the previous message.

 

In the commits tab, it should list the files that were changed (but it doesn't)

 

So, I posted the link of the commit into the messages at the bottom.

 

-Robin

Attachments

    Outcomes