2008-07-10 04:36:12     skyeye

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-07-10 04:36:12     skyeye

heni hbaieb (TUNISIA)

Message: 58604   

 

About emulation skyeye

I have downloaded version skyeye-testsuite-1.2.5

I tried to start the test "skyeye-testsuite-1.2.5/uClinux/bf533"

but when I launch a test for architecture blakfin I get an error in memory addressing itself as a kernel panic case

ok here is the message display:

 

 

skyeye-testsuite-1.2.5/uClinux/bf533$ skyeye -e linux

Your elf file is little endian.

arch: blackfin

mach info: name bf533, mach_init addr 0x80bb5e2

uart_mod:0, desc_in:, desc_out:, converter:

start addr is set to 0x00001000 by exec file.

▒Linux version 2.6.12.1-BFIN-2005R4-ksh (ksh@ksh) (gcc version 3.4.4 (Blackfin 05R4 20051205)) #15 Sun Feb 4 20:14:15 EST 2007

Blackfin support (C) 2004 Analog Devices, Inc.

ADSP-BF533 Rev. 0.0

Warning: Unsupported Chip Revision ADSP-BF533 Rev. 0.0 detected

uClinux/BF533

Blackfin uClinux support by blackfin.uclinux.org

Processor Speed: 110 MHz core clock and 22 Mhz System Clock

Board Memory: 128MB

Memory map:

  text = 0x001000-0x08219c

  data = 0x08cf14-0x0a50bc

  bss = 0x0a50c0-0x0aff04

  rootfs = 0x7f00000-0x7f00000

  stack = 0x08e000-0x090000

Hardware Trace Enabled

Built 1 zonelists

Kernel command line:

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 512 (order: 9, 8192 bytes)

Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)

Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)

Physical pages: 7f00

Memory available: 128128k/130508k RAM, (39k init code, 516k kernel code, 139k data, 1024k dma)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin DATA_A SRAM: 32 KB

Blackfin DATA_B SRAM: 32 KB

Security Framework v1.0.0 initialized

Capability LSM initialized

Mount-cache hash table entries: 512

Linux NoNET1.0 for Linux 2.6

Blackfin DMA Controller for BF533

stamp_init(): registering device resources

BlackFin BF533 serial driver version 2.00 With DMA Support

io scheduler noop registered

io scheduler cfq registered

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

uclinux[mtd]: RAM probe address=0x7f00000 size=0x0

Creating 1 MTD partitions on "RAM":

0x00000000-0x00000000 : "EXT2fs"

mtd: partition "EXT2fs" is out of reach -- disabled

uclinux[mtd0]: set EXT2fs to be root filesystem

end_request: I/O error, dev mtdblock0, sector 2

EXT2-fs: unable to read superblock

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(31,0)

 

TranslateQuoteReplyEditDelete

 

 

2008-07-11 04:04:52     Re: skyeye

Yi Li (CHINA)

Message: 58663   

 

We did not test/update skyeye on blackfin for a long time.

Attachments

    Outcomes