2007-05-25 13:36:18     ERROR: Unable to set frequency to 44100, errno=25

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2007-05-25 13:36:18     ERROR: Unable to set frequency to 44100, errno=25

pengcheng liu (UNITED STATES)

Message: 35627    I was trying to test the AD1836A card in bf537-stamp board

 

the testing sound is a record mp3 file with frequency 44100.

 

when I do mp3play test.mp3

 

it give me this error code:

 

ERROR: Unable to set frequency to 44100, errno=25

 

and I also tried another file tong.mp3 which is directly downloaded from web

 

not work neither, give me a same error but with a different frenquency 11200

 

did any one how solve this problem?

 

thanks

 

waiting for answers online

QuoteReplyEditDelete

 

 

2007-05-25 15:48:48     Re: ERROR: Unable to set frequency to 44100, errno=25

pengcheng liu (UNITED STATES)

Message: 35631    I find the problem is missing something else

 

 

when I do command  ls -l /proc/asound/ad1836/

 

it shows :

 

-r--r--r--    1 root     root            0 Jan  1 01:51 id

-rw-r--r--    1 root     root            0 Jan  1 01:51 oss_mixer

dr-xr-xr-x    3 root     root            0 Jan  1 01:51 pcm0c

dr-xr-xr-x    5 root     root            0 Jan  1 01:51 pcm0p

-rw-r--r--    1 root     root            0 Jan  1 01:51 registers

 

looks like  I am missing another 3 things which should be

<pre class="code">-r--r--r-- 1 0 0 0 id

-rw-r--r-- 1 0 0 0 oss_mixer

dr-xr-xr-x 3 0 0 0 pcm0c

dr-xr-xr-x 3 0 0 0 pcm0p

-rw-r--r-- 1 0 0 0 registers

-r--r--r-- 1 0 0 0 spi

-r--r--r-- 1 0 0 0 sport

-rw-r--r-- 1 0 0 0 talktrough can anyone help me with that?

 

thanks

QuoteReplyEditDelete

 

 

2007-05-25 16:52:10     Re: ERROR: Unable to set frequency to 44100, errno=25

Robin Getz (UNITED STATES)

Message: 35632   

How did you compile the audio driver? (statically into the kernel or as a module?)

 

There should be some help at:

 

http://docs.blackfin.uclinux.org/doku.php?id=ad1836a_setup

 

-Robin

QuoteReplyEditDelete

 

 

2007-05-25 17:31:02     Re: ERROR: Unable to set frequency to 44100, errno=25

pengcheng liu (UNITED STATES)

Message: 35633    I tried both way first as a module then into kernel but no success.

 

I was following the instructions per the website : http://docs.blackfin.uclinux.org/doku.php?id=ad1836a_setup

 

It seems that the spi bus is not being offered under drivers my only selectable SPI options are :

< > Bitbanging SPI master                                                                                   │ │

 

All other SPI options are unavailable to me under the SPI menu option.

 

For Character devices, I have the following two SPORT / SPI related options set :

[*] Blackfin BF53x ADSP SPI ADC support

[*] Blackfin BF53x SPORT support

 

I am using svn version 3174 of the linux-kernel.

 

thanks,

pengcheng

QuoteReplyEditDelete

 

 

2007-05-28 10:55:42     Re: ERROR: Unable to set frequency to 44100, errno=25

pengcheng liu (UNITED STATES)

Message: 35687    hi, Robin

 

I still can not get the AD1836 work properly

 

please give me help on this

 

thanks in advance

 

pengcheng

QuoteReplyEditDelete

 

 

2007-05-30 17:39:35     Re: ERROR: Unable to set frequency to 44100, errno=25

Mike Frysinger (UNITED STATES)

Message: 35802    did you enable all of the backwards OSS compatibility features in your kernel ?  mp3play only works with the old OSS interface, not the new ALSA interface

QuoteReplyEditDelete

 

 

2007-05-30 17:40:13     Re: ERROR: Unable to set frequency to 44100, errno=25

Mike Frysinger (UNITED STATES)

Message: 35803    also, make sure the simple `tone` application works before you try testing with mp3s

QuoteReplyEditDelete

 

 

2008-07-07 22:09:44     回复: ERROR: Unable to set frequency to 44100, errno=25

Xujie Liu (CHINA)

Message: 58462   

 

I enconuterd the same problem, anyone has solved that ? Please tell me the method. Thanks!

 

Best Regards

TranslateQuoteReplyEditDelete

 

 

2008-07-07 22:53:59     Re: 回复: ERROR: Unable to set frequency to 44100, errno=25

Yi Li (CHINA)

Message: 58463   

 

What is your kernel version? Audio Driver? Are you using mp3play? We need all the information to reproduce.

Attachments

    Outcomes