2008-07-03 03:48:00     Jthread does not support bfin compiler, does it?

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-07-03 03:48:00     Jthread does not support bfin compiler, does it?

Matthew Wang (CHINA)

Message: 58249   

 

I wanna use JRTPLIB and Jthread

 

JRTPLIB can be cross-compiled by bfin compiler,

 

but JThread may not, here is the message I got:

 

[root@localhost jthread-1.2.1]# ./configure --host=bfin-linux-uclibc

configure: WARNING: If you wanted to set the --build type, don't use --host.

    If a cross compiler is detected then cross compile mode will be used.

checking for a BSD-compatible install... /usr/bin/install -c

checking whether build environment is sane... yes

checking for gawk... gawk

checking whether make sets $(MAKE)... yes

checking for bfin-linux-uclibc-strip... bfin-linux-uclibc-strip

checking build system type... i686-pc-linux-gnu

checking host system type... Invalid configuration `bfin-linux-uclibc': machine `bfin' not recognized

configure: error: /bin/sh ./config.sub bfin-linux-uclibc failed

[root@localhost jthread-1.2.1]#

 

 

[root@localhost jthread-1.2.1]# ./configure --host=bfin-uclinux

configure: WARNING: If you wanted to set the --build type, don't use --host.

    If a cross compiler is detected then cross compile mode will be used.

checking for a BSD-compatible install... /usr/bin/install -c

checking whether build environment is sane... yes

checking for gawk... gawk

checking whether make sets $(MAKE)... yes

checking for bfin-uclinux-strip... bfin-uclinux-strip

checking build system type... i686-pc-linux-gnu

checking host system type... Invalid configuration `bfin-uclinux': machine `bfin' not recognized

configure: error: /bin/sh ./config.sub bfin-uclinux failed

[root@localhost jthread-1.2.1]#

TranslateQuoteReplyEditDelete

 

 

2008-07-03 08:20:35     Re: Jthread does not support bfin compiler, does it?

Mike Frysinger (UNITED STATES)

Message: 58268   

 

please read the FAQ (Running config.sub results in "machine `bfin' not recognized"):

http://docs.blackfin.uclinux.org/doku.php?id=faq

QuoteReplyEditDelete

 

 

2008-07-03 21:56:17     回复: Re: Jthread does not support bfin compiler, does it?

Matthew Wang (CHINA)

Message: 58297   

 

Mike, thank u for ur help~~~

 

I got it~~~

 

 

 

Matthew

Attachments

    Outcomes