2008-07-02 03:05:28     Kernal compilation

Document created by Aaronwu Employee on Aug 7, 2013
Version 1Show Document
  • View in full screen mode

2008-07-02 03:05:28     Kernal compilation

mahima k (INDIA)

Message: 58178   

 

Hi

 

 

 

I am Mahi,i have enabled the USB   - ISP1362 in UClinux distribution by giving the command make menuconfig...The problem is ,ISP1362 device driver program is not adding into kernal ,i am getting following error.....any one guide me how can i eliminate this error...

 

 

 

  OBJCOPY arch/blackfin/boot/vmlinux.bin

  GZIP    arch/blackfin/boot/vmlinux.gz

  UIMAGE  arch/blackfin/boot/vmImage

Image Name:   Linux-2.6.19.3-ADI-2007R1-svn

Created:      Wed Jul  2 12:32:52 2008

Image Type:   Blackfin Linux Kernel Image (gzip compressed)

Data Size:    770430 Bytes = 752.37 kB = 0.73 MB

Load Address: 0x00001000

Entry Point:  0x00001000

Kernel: arch/blackfin/boot/vmImage is ready

  Building modules, stage 2.

  MODPOST 17 modules

WARNING: "usb_alloc_dev" [drivers/usb/host/isp1362-hcd.ko] undefined!

make[2]: *** [__modpost] Error 1

make[1]: *** [modules] Error 2

make[1]: Leaving directory `/work_15.12.07/work/uClinux-dist/linux-2.6.x'

make: *** [linux] Error 1

 

 

 

 

with regards

 

mahi

QuoteReplyEditDelete

 

 

2008-07-02 03:55:04     Re: Kernal compilation

Yi Li (CHINA)

Message: 58183   

 

pleasse refer to: http://docs.blackfin.uclinux.org/doku.php?id=hw:cards:usb_ez-extender

Attachments

    Outcomes