2008-06-30 01:31:06     Regarding microSD

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-30 01:31:06     Regarding microSD

V Hemanth Kumar (INDIA)

Message: 58061   

 

Hi,

 

The distribution & http://docs.blackfin.uclinux.org/ online document says MMC & SD cards work fine.

 

As we know that mmc & microSD differ in the pins, initialization sequence, internal registers, command/response format.

 

So does the microSD card works fine with the available MMC/SD card drivers?

 

or Does it require changes or seperate driver to be developed?

 

Regards,

 

Hemanth Kumar.V

 

 

 

QuoteReplyEditDelete

 

 

2008-06-30 03:13:53     Re: Regarding microSD

Yi Li (CHINA)

Message: 58062   

 

Do you mean the SPI-MMC driver or BF54x SD host driver? AFAIK, we did't test microSD using these two drivers.

QuoteReplyEditDelete

 

 

2008-06-30 05:34:52     Re: Regarding microSD

V Hemanth Kumar (INDIA)

Message: 58104      

 

Thanks for the response Yi Li.

 

I was referring to SPI-MMC driver.

 

We are using the BF527EZ Kit & planning to test the microSD.

 

So is it possible to provide a microSD slot on the expansion interface of the Ezkit?

 

 

 

QuoteReplyEditDelete

 

 

2008-06-30 06:03:30     Re: Regarding microSD

Mike Frysinger (UNITED STATES)

Message: 58107   

 

we've never tested the SD slot on the bf527 ezkit

QuoteReplyEditDelete

 

 

2008-06-30 10:01:43     Re: Regarding microSD

V Hemanth Kumar (INDIA)

Message: 58125   

 

Hi Mike,

 

In the BF527 EZKit board I could not figure out the SD slot, and in the "BF527 EZKIT Lite System Manual" nothing is mentioned about the SD slot.

 

So my question below is(could be weird one, but please bear with me):-

 

1. Can we interface/connect the microSD slot to the EZKIT's expansion interface (with help of our Hardware engineers)?

 

What I mean is, there is a SPI connector (P9) interface, so can we connect the microSD slot to this connector?

 

2. Based on your yes or no response, further clarifications will help us.

 

Thanks.

QuoteReplyEditDelete

 

 

2008-06-30 10:56:52     Re: Regarding microSD

Mike Frysinger (UNITED STATES)

Message: 58127   

 

it seems the SD slot has been dropped ... my newer boards dont have it at all

 

i cant tell you a thing about the physical aspects of it since there is no documentation ... better you just pretend it isnt there

 

the BF52x has no SD host controller (unlike the BF54x), so if you want to control a SD, you should look at the SD/MMC/SPI examples

Attachments

Outcomes