2008-06-27 06:17:53     Telnet for BF357E uClinux-dist2008R1-RC8

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-27 06:17:53     Telnet for BF357E uClinux-dist2008R1-RC8

tom R (FRANCE)

Message: 57961   

 

    Hello!!

 

If someone has even resolved this problem, plz help me! I work on a BF537E,  uClinux-dist2008R1-RC8 and the command the command "telnet 192.168.0.97" gives me the following errors:

 

telnetd: All network ports in use.

Connection closed by foreign host.

 

 

According to the tutorial, I made the following configuration:

 

grep TELNET config/.config

CONFIG_USER_TELNETD_TELNETD=y

CONFIG_USER_TELNETD_DOES_NOT_USE_OPENPTY=y

CONFIG_USER_TELNET_TELNET=y

# CONFIG_USER_BUSYBOX_TELNET is not set

# CONFIG_USER_BUSYBOX_TELNETD is not set

 

 

# on the development system

 

ls -l romfs/bin/telnetd

-rwxr-xr-x 1 isen isen 20116 2008-06-27 11:59 romfs/bin/telnetd

 

# on the target system

 

root:/> ls -l /bin/telnet

 

-rwxr-xr-x         1  1000        1000           20116 Jun   27   2008   /bin/telnetd

 

# On the target

 

root:/> cat /etc/inetd.conf

 

shell     stream tcp nowait root   /bin/rshd

 

telnet   stream tcp nowait root   /bin/telnetd

 

root:/> telnetd

 

telnetd: getpeername: Socket operation on non-socket

 

telnetd: All network ports in use

 

 

 

The Bf server ip is 192.168.0.97 and my station's is 192.168.0.98.

 

Thanks!

 

 

TranslateQuoteReplyEditDelete

 

 

2008-06-27 06:32:40     Re: Telnet for BF357E uClinux-dist2008R1-RC8

Yi Li (CHINA)

Message: 57962   

 

Please search this forum.

 

check your the /dev/ on your board, do you have /dev/ptmx, /dev/pts/. If not, enable "CONFIG_UNIX98_PTYS ".

QuoteReplyEditDelete

 

 

2008-06-27 08:07:23     Re: Telnet for BF357E uClinux-dist2008R1-RC8

tom R (FRANCE)

Message: 57963   

 

There is a /dev/pts0 and a pts1, but no /dev/ptmx. My "CONFIG_UNIX98_PTYS " is already enable.

 

So, I copied the line which contain ptmx in device_table.txt to device_table_min. It's work! Thank you!

Attachments

    Outcomes