2008-06-25 04:28:07     using eclipse with blackfin toolchain

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-25 04:28:07     using eclipse with blackfin toolchain

Juhi Sinha (INDIA)

Message: 57831   

 

We are trying to debug and run programs on eclipse using blackfin toolchains. We have downloaded the required plugins from

 

<a rel="nofollow" title="http://blackfin.uclinux.org/eclipse/" class="urlextern" href="../../eclipse/">http://blackfin.uclinux.org/eclipse/ . We are able to debug the programs using ' linux GCC ' toolchain but we are not able to use blackfin toolchain .

 

When we tried to build a small 'hello world' example we got following errors :

 

-------------------------------------------------------------------------------------------------------------

 

**** Rebuild of configuration Debug for project wed25_4 ****

 

**** Internal Builder is used for build               ****

****  WARNING: The "Debug" Configuration may not build  ****

****  because it uses the "Blackfin Linux FLAT (bfin-uclinux)"  ****

****  tool-chain that is unsupported on this system.  ****

 

****  Attempting to build...  ****

 

Nothing to build for wed25_4

 

--------------------------------------------------------------------------------------------------------------

 

Moreover 'makefile' is not made automatically.

 

Also in

 

project properties--> 'C/C++ Build' -->It says that "This configuration support is not installed on this system" .

 

Do we have to install something else besides those blackfin plugins ??

 

Please guide us with this !!

 

 

QuoteReplyEditDelete

 

 

2008-06-25 08:12:11     Re: using eclipse with blackfin toolchain

Mike Frysinger (UNITED STATES)

Message: 57858   

 

the toolchain wont work if it isnt in your PATH

 

QuoteReplyEditDelete

 

 

2008-06-25 08:29:26     Re: using eclipse with blackfin toolchain

Juhi Sinha (INDIA)

Message: 57859   

 

We have included the toolchain in our path but still we are not able to run our program.

 

We are now able to build it but when we try to debug the process is terminated and  we get an error :

 

"gdb/mi(suspended) <you can't do that without a process to debug >"

Attachments

    Outcomes