2008-06-22 22:05:08     561 and isp1362

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-22 22:05:08     561 and isp1362

sima sima (UNITED STATES)

Message: 57691   

 

Hi everyone:

 

I am working with  BF561 EZKIT board with Linux version 2.6.16.11 (2006R1)& USB Extender add on card for isp1362. I have selected PF46 for GPIO interrupt. when I connect a USB pan ,I got some problems

 

I have pasted the displayed messages below. Please suggest.

 

CPU:   ADSP bf561-0.3 (Detected Rev: 0.5)

Board:  BF561 Easyview board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 575 MHz, Core: 575 MHz, System: 143 MHz

RAM:   128 MB

Flash: 16 MB

In:    serial

Out:   serial

Err:   serial

NAND:  256 MiB

Net:   MAC:   00:89:77:88:89:88

Hit any key to stop autoboot:  0

u-boot> run nfsboot

Found DM9000 or dm9010 ID:90000a46 at address 2c000000 !

DM9000 work in 16 bus width

PHY is autonegotiating now, pls waiting ...

operating at 100M full duplex mode

[eth_init]MAC  00  89  77  88  89  88

TFTP from server 192.168.7.45; our IP address is 192.168.7.233

Filename 'uImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################

done

Bytes transferred = 3241384 (3175a8 hex)

## Booting image at 01000000 ...

   Image Name:   uClinux Kernel and Filesystem

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3241320 Bytes =  3.1 MB

   Load Address: 00100000

   Entry Point:  00100000

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... **********************************************

********************************************************************************

********************************************************************************

************************OK

Starting Kernel at = 100000

﨤inux version 2.6.16.11.ADI-2006R1blackfin (root@localhost.localdomain) (gcc ve

rsion 3.4.5 (ADI 2006R1)) #500 Thu Jun 19 22:25:53 CST 2008

The value of AEC IC mic_pgagain is 0x3005

MTD_SIZE = 0x1100000!

Blackfin support (C) 2004 Analog Devices, Inc.

ADSP-BF561 Rev. 0.1280

uClinux/BF561

Blackfin uClinux support by blackfin.uclinux.org

Processor Speed: 575 MHz core clock and 143 Mhz System Clock

Board Memory: 45MB

Memory map:

  text = 0x100000-0x260b80

  data = 0x27bb6c-0x2af1bc

  bss  = 0x2af1c0-0x349df4

  memory = 0x34a000-0x1b00000

  rootfs = 0x1b00000-0x2c00000

  stack = 0x27c000-0x27e000

Command line: 'root=/dev/mtdblock0 rw'

Instruction Cache Enabled

Data Cache Enabled (write-through)

Hardware Trace Enabled

Built 1 zonelists

Kernel command line: root=/dev/mtdblock0 rw

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 128 (order: 7, 2048 bytes)

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Physical pages: 1b00

Memory available: 24024k/43537k RAM, (52k init code, 1410k kernel code, 619k dat

a, 18432k dma)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin DATA_A SRAM: 16 KB

Blackfin DATA_B SRAM: 16 KB

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin DMA Controller for BF561

bfin_isp1362_init(): registering device resources

SCSI subsystem initialized

usbcore: registered new driver usbfs

usbcore: registered new driver hub

NTFS driver 2.1.26 [Flags: R/W DEBUG].

JFFS2 version 2.2. (NAND) (C) 2001-2003 Red Hat, Inc.

yaffs Jun 18 2008 22:51:58 Installing.

io scheduler noop registered

io scheduler anticipatory registered

io scheduler cfq registered (default)

ADI Video Driver v1.10e

Programming ADV7181...

Configured for ADV7181B

PAL Camera found [4]

ADI KeyPad Driver v1.10e

ADI Audio Driver v1.45e

Configuring Audio Ineterrupts...

Audio: IRQ 71 is installed successfully.

Audio: IRQ 30 is installed successfully.

enable_irq(71) unbalanced from 001b2340

enable_irq(30) unbalanced from 001b2346

Configuring Audio Ineterrupts completed

Core B Loader Module enabled

LcdDriver v1.10e

BlackFin BF533 serial driver version 2.00 With DMA Support

RAMDISK driver initialized: 8 RAM disks of 4096K size 1024 blocksize

usbcore: registered new driver ub

Starting to initiate DM9000A...

<DM9KS> I/O: 2c000000, VID: 90000a46

id_val=0

PPP generic driver version 2.4.2

uclinux[mtd]: RAM probe address=0x1b00000 size=0x1100000

Creating 1 MTD partitions on "RAM":

0x00000000-0x01100000 : "EXT2fs"

uclinux[mtd]: set EXT2fs to be root filesystem

BF5xx flash: probing 16-bit flash bus

BF5xx flash: Found 1 x16 devices at 0x0 in 16-bit bank

Amd/Fujitsu Extended Query Table at 0x0040

BF5xx flash: CFI does not contain boot bank location. Assuming top.

number of CFI chips: 1

cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.

Using static partition definition

Creating 4 MTD partitions on "BF5xx flash":

0x00000000-0x00080000 : "Bootloader"

0x00080000-0x00700000 : "Kernel1"

0x00700000-0x00e00000 : "Kernel2"

0x00e00000-0x01000000 : "JFFS2"

NAND device: Manufacturer ID: 0xec, Chip ID: 0xda (Samsung NAND 256MiB 3,3V 8-bi

t)

Scanning device for bad blocks

Bad eraseblock 257 at 0x02020000

Bad eraseblock 1370 at 0x0ab40000

Bad eraseblock 1690 at 0x0d340000

Creating 2 MTD partitions on "NAND 256MiB 3,3V 8-bit":

0x00000000-0x02000000 : "Userinfo"

0x02000000-0x40000000 : "Yaffs"

mtd: partition "Yaffs" extends beyond the end of device "NAND 256MiB 3,3V 8-bit"

-- size truncated to 0xe000000

usbmon: debugfs is not available

driver isp1362-hcd, 2005-04-04

Blackfin GPIO interrupt setup: flag PF46, irq 58

isp1362-hcd isp1362-hcd.0: ISP1362 Host Controller

isp1362-hcd isp1362-hcd.0: new USB bus registered, assigned bus number 1

isp1362_hc_reset:

isp1362-hcd isp1362-hcd.0: irq 58, io mem 0x28000000

isp1362_hc_start:

isp1362-hcd isp1362-hcd.0: ISP1362 Memory usage:

isp1362-hcd isp1362-hcd.0:   ISTL:    2 *  256:      512 @ $0000:$0100

isp1362-hcd isp1362-hcd.0:   INTL:   16 * ( 64+8):  1152 @ $0200

isp1362-hcd isp1362-hcd.0:   ATL :   32 * ( 64+8):  2304 @ $0680

isp1362-hcd isp1362-hcd.0:   USED/FREE:   3968       128

usb usb1: Product: ISP1362 Host Controller

usb usb1: Manufacturer: Linux 2.6.16.11.ADI-2006R1blackfin isp1362-hcd

usb usb1: SerialNumber: isp1362-hcd.0

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 2 ports detected

ISP1362 Host Controller, irq 58

Initializing USB Mass Storage driver...

usbcore: registered new driver usb-storage

USB Mass Storage support registered.

NET: Registered protocol family 2

IP route cache hash table entries: 256 (order: -2, 1024 bytes)

TCP established hash table entries: 1024 (order: 0, 4096 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 1024 bind 1024)

TCP reno registered

TCP bic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

802.1Q VLAN Support v1.8 Ben Greear <greearb@candelatech.com>

All bugs added by David S. Miller <davem@redhat.com>

VFS: Mounted root (ext2 filesystem).

Freeing unused kernel memory: 52k freed (0x261000 - 0x26d000)

dma_alloc_init: dma_page @ 0x01af6000 - 256 pages at 0x02c00000

yaffs: dev is 32505861 name is "mtdblock5"

yaffs: Attempting MTD mount on 31.5, "mtdblock5"

yaffs: auto selecting yaffs2

yaffs: dev is 32505862 name is "mtdblock6"

yaffs: Attempting MTD mount on 31.6, "mtdblock6"

yaffs: auto selecting yaffs2

block 2 is bad

block 1115 is bad

block 1435 is bad

Set eth0 to MAC address 00:73:25:69:98:e5

Easyview ethernet interrupt setup.

Spent 6412 ms to negotiate, Operating at unknown: 15, 16 bus width mode

PPPoE options file exits in flash

I am setting local IP

 

Welcome to:

       ____ _  _

      /  __| ||_|             _  _

_   _| |  | | _ ____  _   _ \ \/ /

| | | | |  | || |  _ \| | | | \  /

| |_| | |__| || | | | | |_| | /  \

|  ___\____|_||_|_| |_|\____|/_/\_\

|_|

 

For further information see:

http://www.uclinux.org/

http://blackfin.uclinux.org/

 

********************************************************************************

***

*****************************       IMAGE III         **************************

***

********************************************************************************

***

 

 

BusyBox v1.00 (2007.04.11-12:22+0000) Built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:~> //( now I insert a USB pan and got the following message)

 

usb 1-2: new full speed USB device using isp1362-hcd and address 2

usb 1-2: device descriptor read/64, error -110

usb 1-2: device descriptor read/64, error -110

usb 1-2: new full speed USB device using isp1362-hcd and address 3

usb 1-2: device descriptor read/64, error -110

usb 1-2: new full speed USB device using isp1362-hcd and address 4

usb 1-2: device descriptor read/64, error -110

usb 1-2: new full speed USB device using isp1362-hcd and address 5

usb 1-2: device descriptor read/64, error -110

usb 1-2: device descriptor read/64, error -110

 

 

I know the error -110 is meaning time out ,and i measured the pin 38 CLKOUT of the isp1362,I got a 12M clock frequency.

 

 

Thanks a lot!

Attachments

    Outcomes